Issue
Once a Modicon Edge I/O NTS distributed system is configured using the configurator or the web interface, the next step is to download the configuration into the target hardware. At this stage, there may be input/output modules that are part of the detected hardware using an older firmware version that is not compatible. To overcome this configuration mismatch, an update of the firmware of the existing modules is required.
Resolution
The purpose of this article is to show how to perform bulk firmware update for input/output modules ...
Disclaimer
The views and opinions expressed in this article are those of the author(s) and do not necessarily reflect the official policy or position of Schneider Electric.