Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Remote update of M172P* application

HVAC and Pumping Forum

Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
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
  • Industrial Automation
  • HVAC and Pumping Forum
  • Remote update of M172P* application
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
FedericoM
FedericoM Mentor
119
Bastian_Schmitz
Bastian_Schmitz Champion
64
M_Cervati
M_Cervati Troubleshooter
18
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Related Products
product field
Schneider Electric
EcoStruxure™ Machine Expert - HVAC

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to HVAC and Pumping Forum
Start a Topic
Solved
obscuresc
obscuresc
Troubleshooter

Posted: ‎2023-10-02 10:02 PM

0 Likes
9
3021
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
Posted: ‎2023-10-02 10:02 PM

Remote update of M172P* application

Hi,

 

I am currently using devices in the M172P* range with EcoStruxure Machine Expert - HVAC.

I have been updating these PLCs remotely via Modbus TCP.

So far, the experience is less than ideal, taking ~40 minutes to perform an update, and occasionally dropping out and having to restart from the beginning.

This process is also one-to-one, and hence, can't readily update multiple PLCs at once.

 

FTP is also less than ideal, as you can't update PARAM.* files (per advice from tech support), hence a 'complete' 'Download All' equivalent via ESME HVAC is not possible. You must also force a reboot (via other means) of the PLC in order for the application upload to take effect.

 

Is there a better method to federate software updates in a scalable manner? If not, is there a means that we replicate the software update process with a single board computer (Linux-based) (i.e we use Modbus through the Mini USB port)? In this way, we could create something scalable ourselves.

 

Thanks,

Jack

 

 

 

Labels
  • Labels:
  • HVAC
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
FedericoM
FedericoM Mentor
Mentor

Posted: ‎2023-10-05 02:39 AM

In response to obscuresc
0 Likes
0
2978
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
Posted: ‎2023-10-05 02:39 AM

The info related to how projects are downloaded is not public.

About the download time improvement, sorry I can't give you an exact roadmap, my guess is Q2

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 9
FedericoM
FedericoM Mentor
Mentor

Posted: ‎2023-10-04 01:47 AM . Last Modified: ‎2023-10-04 01:49 AM

0 Likes
0
3010
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
Posted: ‎2023-10-04 01:47 AM . Last Modified: ‎2023-10-04 01:49 AM

Hello,

 

not in the next release of ESME HVAC, but I hope next year will implement an improvement of the download times via modbus/Tcp (it's in the roadmap).

 

At the moment I can suggest:

- download from Installer only what is really needed in terms of update among Application, Local and Remote Display

- via FTP you can transfer a file with the format of a PARAM.DAT file which could be loaded by your project using sysUsbFileName and sysUsbCommand=116

 

Download times depends also on the CPU load of your application and the network band, so if you add a kind of option in your project which basically reduce the load of timed task...you should see some time improvement.

 

At least today, it's not possible to run ESME HVAC core on linux based OS.

 

Reply

Link copied. Please paste this link to share this article on your social media post.

otrotabi
otrotabi
Contributor

Posted: ‎2023-10-04 04:06 AM

0 Likes
0
3003
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
Posted: ‎2023-10-04 04:06 AM

Hello, thanks for sharing this. I think most of us share your thoughts. Could you further describe your current setup that allows you to  remotely access the PLCs? You have the PLCs connected to the local network and a port opened on a router ? If that is so, which ports need to be opened ?

 

I am also curious why you are mentioning that a reboot is needed... Isn´t that needed also with local updates as well ? It would not surprise me that some day in the future changes in software could be done without a reboot needed, but in terms of the controlled machine status, that looks harder to solve.

 

I´ve never had the time to give this https://thesecmaster.com/step-by-step-procedure-to-install-windows-10-on-a-raspberry-pi-4/ a try (there are many of these posts on internet, this happened to be one of the first that came up) but it looks like it is possible to setup windows 10 or 11 on a Raspberry Pi. I am aware of the eventual security issues that might represent (as well as probably extra cost, I do not know if Microsoft gives this Windows setup for free). Anyway, having an interface to be able to connect to the M172 line from Linux would be great !

Reply

Link copied. Please paste this link to share this article on your social media post.

FedericoM
FedericoM Mentor
Mentor

Posted: ‎2023-10-04 05:07 AM

0 Likes
2
3000
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
Posted: ‎2023-10-04 05:07 AM

A reboot of PLC is needed whenever you change something in the Client configuration of Modbus, I/O expansion allocations and BACnet (in terms of # of objects) in the configuration side.

These settings are reloaded only at boot.

 

Unless using a M172 Secure Interface, a Harmony ST6 or some other device providing a VPN, you need to know the public IP of the router to which M172 is connected and enable a port forwarding of port 502 of the router to the 502 of M172

Reply

Link copied. Please paste this link to share this article on your social media post.

otrotabi
otrotabi
Contributor

Posted: ‎2023-10-04 06:00 AM

In response to FedericoM
0 Likes
1
2980
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
Posted: ‎2023-10-04 06:00 AM

Thanks.  So, basically this is it ?

 

network.jpg

However, I am missing the point regarding the reboot. What is different if local or remote control ? 

Reply

Link copied. Please paste this link to share this article on your social media post.

obscuresc
obscuresc
Troubleshooter

Posted: ‎2023-10-04 03:56 PM

0 Likes
1
2982
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
Posted: ‎2023-10-04 03:56 PM

Hi all,

 

@FedericoM thanks for the update. Is the roadmap available for us to see? I sometimes pause application while loading. I suspect most of the delay is made up by latency due to the polling nature of Modbus and that a single poll doesn't move that much data. If I had loaded all files via FTP, and used 'sysUsbCommand', can I update everything? Regarding Linux-based computer question, I meant, could we emulate the way EcoStruxure pushes the data through Modbus for an update? If we can, we can update very readily, and in a scalable manner.

 

@otrotabi we use an industrial router with a VPN service with a port for Modbus set open. We very much like the idea of a Raspberry Pi, but don't want Windows on it. Because you can update via Modbus, if we can the specs on how an update is performed, we could emulate it at the edge, and not require a user-oriented connection to all our field units.

 

Thanks,

Jack

 

Reply

Link copied. Please paste this link to share this article on your social media post.

FedericoM
FedericoM Mentor
Mentor

Posted: ‎2023-10-05 02:39 AM

In response to obscuresc
0 Likes
0
2979
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
Posted: ‎2023-10-05 02:39 AM

The info related to how projects are downloaded is not public.

About the download time improvement, sorry I can't give you an exact roadmap, my guess is Q2

Reply

Link copied. Please paste this link to share this article on your social media post.

FedericoM
FedericoM Mentor
Mentor

Posted: ‎2023-10-05 02:51 AM

In response to otrotabi
0 Likes
0
2977
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
Posted: ‎2023-10-05 02:51 AM

No differences between remote and local download, a download all requires always a reboot if you changed something in the Client configuration of Modbus, I/O expansion allocations and BACnet (in terms of # of objects) in the configuration side

Reply

Link copied. Please paste this link to share this article on your social media post.

obscuresc
obscuresc
Troubleshooter

Posted: ‎2023-10-08 08:06 PM

0 Likes
0
2946
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
Posted: ‎2023-10-08 08:06 PM

@FedericoM Is it possible to open the specification for project download?

Reply

Link copied. Please paste this link to share this article on your social media post.

FedericoM
FedericoM Mentor
Mentor

Posted: ‎2023-10-09 01:22 AM

1 Like
0
2942
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
Posted: ‎2023-10-09 01:22 AM

Sorry but I haven't the rights to do that
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.