Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Parametric input and output configuration TM172

HVAC and Pumping Forum

Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
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
  • Industrial Automation
  • HVAC and Pumping Forum
  • Parametric input and output configuration TM172
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
FedericoM
FedericoM Mentor
119
Bastian_Schmitz
Bastian_Schmitz Champion
64
M_Cervati
M_Cervati Troubleshooter
18
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to HVAC and Pumping Forum
Start a Topic
Solved
otrotabi
otrotabi
Contributor

Posted: ‎2024-10-15 04:27 AM . Last Modified: ‎2024-10-15 04:28 AM

0 Likes
2
1510
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
Posted: ‎2024-10-15 04:27 AM . Last Modified: ‎2024-10-15 04:28 AM

Parametric input and output configuration TM172

I am trying to develop a project where I can freely define which input gets assigned to a specific function by using an EEPROM variable, within a certain number of choices. The same criterion should work also for the outputs.

 

This is based on how Dixell allows you freely define inputs and outputs on their IC100 and IC200 chiller controllers.

 

I attach here a work in progress test project. I have not done anything on a real PLC yet. I wrote a FB which has the outputs from the different logical FB (for example CompCntrl_OnOff) as inputs, as well as all the EEPROM configuration variables. I have not done anything yet regarding input assignments but should be similar.

 

Although for a different purpose, this works similar to the SR_Params program used in the air-water cooled chiller for large machines TDVA. I noticed SR_Params is included inside the background tasks.

 

So my questions are: 

 

1) Is there any easier way ? I know I could use some string function to output a string with contents "DOL1" for example. How about memory notation for the outputs (MW.xxxx) ?

2) Can this work ? Or would it impose an extra overload on the program that would possibly crash it ?

3) What about assigning this program to the background tasks ? Mi idea is that if the user enters the configuration mode in order to change the configuration variables, machine execution should stop. So actually once the configuration is done when the machine is set up, outputs and inputs assignment would actually never change.

 

This is how the program looks like graphically. FB_assignment assigns for example xMQ_Compressor to DO_ixDOL1 if OutCfg_usilDol1 = 10

 

otrotabi_1-1728991459780.png

otrotabi_0-1728990280534.png

 

Attachments
ParametricIO.zip
Labels
  • Labels:
  • HVAC
  • Tags:
  • ecostruxure
  • english
  • hvac
  • TM172
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Bastian_Schmitz
Bastian_Schmitz Champion
Champion

Posted: ‎2024-10-15 11:05 PM

0 Likes
1
1486
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
Posted: ‎2024-10-15 11:05 PM

The common way to do something like that is to work with pointers. You could see this in the integrated Parametric AHU Project in ESME HVAC. To do anything with string variables is depending on the hardware not a good idea. As example if you use TM171O you will fast get memory problems. If you want to use text in the code for a better understanding use Enumeration instead. 

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
Bastian_Schmitz
Bastian_Schmitz Champion
Champion

Posted: ‎2024-10-15 11:05 PM

0 Likes
1
1487
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
Posted: ‎2024-10-15 11:05 PM

The common way to do something like that is to work with pointers. You could see this in the integrated Parametric AHU Project in ESME HVAC. To do anything with string variables is depending on the hardware not a good idea. As example if you use TM171O you will fast get memory problems. If you want to use text in the code for a better understanding use Enumeration instead. 

Reply

Link copied. Please paste this link to share this article on your social media post.

otrotabi
otrotabi
Contributor

Posted: ‎2024-10-16 04:19 AM

In response to Bastian_Schmitz
0 Likes
0
1473
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
Posted: ‎2024-10-16 04:19 AM

Thanks.  I will study the AHU project in detail.

 

Regards
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.