SCADAPack x70 Modbus Master/Client support for Binary DNP3 packed in Modbus Input / Holding Registers

Geo SCADA and Remote Operations Devices Ideas

Use this portal to submit your innovative ideas to make Geo SCADA Expert and Devices such as SCADAPack, Trio and Realflo of greater value to you and to the SCADA & Telemetry community. Every idea will be individually reviewed by our team for merit and will be marked Under Consideration.
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
  • Remote Operations
  • Geo SCADA and Remote Operations Devices Ideas
  • SCADAPack x70 Modbus Master/Client support for Binary DNP3 packed in Modbus Input / Holding Registers
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Labels
Top Labels
  • Alphabetical
  • SCADA 2
  • ViewX 2
  • Mimics 2
  • SCADAPack 2
  • Scripting 1
  • Virtual ViewX 1
  • Geo SCADA Expert 1
  • Efficiency 1
  • Configuration management 1
  • Modbus to WiStar 1
Idea Statuses
  • Submitted 13
  • Under consideration 126
  • Accepted 1
  • Declined 4
  • Partially delivered 0
  • Delivered 0
  • Abandoned 0
Related Products
Thumbnail of EcoStruxure™ Geo SCADA Expert
Schneider Electric
EcoStruxure™ Geo SCADA Expert
114
Thumbnail of SCADAPack 57x
Schneider Electric
SCADAPack 57x
2
Thumbnail of Accutech
Schneider Electric
Accutech
1
Load more
Completed Ideas
  • Accutech Modbus Master gateway to read Modbus devices and incorporate into WiStar net

  • Controller Key Enhancement

  • Restore "Embed Source Code for Upload" Option in Workbench (SP300 family)

  • DNP Outstation And DNP Master Diagnostics

View All
Top Liked Authors
User Likes Count
tfranklin
Commander tfranklin
15
aosburn
Lieutenant JG aosburn
8
ChrisHinton
Ensign ChrisHinton
1
gabarit
Lieutenant JG gabarit
1
View All

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
0 Likes

SCADAPack x70 Modbus Master/Client support for Binary DNP3 packed in Modbus Input / Holding Registers

Status: Submitted Submitted by Spock BevanWeiss on ‎2021-02-25 08:41 PM
4 Comments (4 New)

The SCADAPack E-Series Modbus Scanner functionality allowed for Holding Registers and Input Registers to be used to store packed digital bits, and for these to still be exposed as DNP3 Binary Points without requiring any additional logic / custom code.  This was a native function of the E-Series Modbus Scanner.

 

In the x70, this functionality appears to have been lost, and now it is not possible to map digital bits in Input / Holding Registers into DNP3 Binary Points.

 

There are a large number of Modbus devices that present all of their data in the Holding Registers, and to have to use custom code in the x70 to map these to DNP3 points is very frustrating.  Even more so when the E-series RTUs did this without an issue.  It seems crazy that a new RTU family (x70) would be so far less functional than the RTU that it is advertised to replace.

 

In the Modbus Scanners dialog it should be possible to select Modbus Data Type: UINT and to select Object Type: Digital

Tags (6)
  • Find more ideas tagged with:
  • english
  • scada
  • SCADA app
  • SCADA software
  • SCADA tutorial
  • Telemetry and SCADA
Comment

Link copied. Please paste this link to share this article on your social media post.

  • Back to Idea Exchange
  • Previous
  • Next
4 Comments
MartinChartrand
Captain MartinChartrand Captain
Captain
‎2021-03-01 05:06 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2021-03-01 05:06 AM
Status changed to: Under consideration

Thank you @BevanWeiss,

I will discuss with the RTU team and get back to you as soon as I can on this request.

Regards,

Martin

 

MartinChartrand
Captain MartinChartrand Captain
Captain
‎2021-03-01 06:52 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2021-03-01 06:52 AM

Hello again,

The good news is that this is scheduled for RemoteConnect 2.6.1.

I do not know when this will happen but will post it once I know for sure.

Regards

M

 

BevanWeiss
Spock BevanWeiss
Spock
‎2021-03-03 03:50 PM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2021-03-03 03:50 PM

Thanks Martin,

Would greatly appreciate if I could be involved in Beta testing of this.

 

We have two projects upcoming where this exact lack in functionality is an issue for us.

One involving communications to a Siemens S7-1500 PLC, and the other to a Schneider M580.

 

They would actually both benefit from some customisable Modbus -> DNP3 'DTM' type mapping actually... where a data structure in the Modbus holding register space could be mapped to a structure of DNP3 points.  Since the Modbus registers typically end up being a mix of digital and different analog types (i.e. 16x digitals, then 2x INTs, then 4x DINTS, then 4x REALS and then the next device is mapped in... so we start from 16x digitals again...), which doesn't align particularly well with the current 1 Modbus scanner row = strictly 1 DNP3 data type.

But... the exact request listed in the original message is a step in the right direction all the same (and would solve the current problem for now)

MartinChartrand
Captain MartinChartrand Captain
Captain
‎2021-03-04 10:10 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2021-03-04 10:10 AM

Hello again,

Yes, we can certainly include you in the beta test of this feature and will contact you when we're ready to proceed.

Thank you again for your interest in improving our products.

Regards,

Martin

Comment
Preview Exit Preview

never-displayed

Hint:
@ links to members, content
 
  • Back to Idea Exchange
  • Previous
  • Next
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.