Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Use this portal to submit your innovative ideas to make Geo SCADA Expert and Devices such as SCADAPack, Trio and Realflo of greater value to you and to the SCADA & Telemetry community. Every idea will be individually reviewed by our team for merit and will be marked Under Consideration.
Search in
| User | Likes Count |
|---|---|
| 7 | |
| 4 | |
| 2 | |
| 1 | |
| 1 |
I would like to suggest a change to the Controller Key feature found in Telepace Studio 5.4.2. I originally submitted this as a bug but because the Controller Key feature prevents writes to the PLC ladder program it was referred to this forum. In summary, changes can be saved to the project when the Telepace editor is exited, which could (under certain circumstances) lead to corruption.
It is true that the ladder program will not be sent to the PLC if the “WRITE” button is not pressed but I suggest two failure scenarios here. Maybe a bit unlikely but I present them for review nonetheless:
First, unexpected changes could be saved to the project by a bad person; if the project is ever opened by an authorised user who actually needs to modify the project, and if all sheets are not checked thoroughly before writing/saving, the legit user could inadvertently commit the hacked changes along with the intended modifications.
Second, the “Controller Lock” tends to imply that the project is secure, at least in my mind. I would prefer that project changes were “bundled” into the controller lock as well as the WRITE commits.
I respectfully suggest that edits to the project are discarded if the Controller Lock is enabled and the "Save changes?" dialog not displayed so that the hacker is not sure what is happening. This would indicate that the Controller Lock feature not only controls the written PLC ladder program but the project as well, which is the same thing just in un-committed form.
I am recommending these two changes to the next possible release of the Telepace editor. The changes would make the editing environment more secure than it already is. Thank you for providing this forum to submit these types of ideas.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.