Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Advanced Modbus driver optimization

Geo SCADA and Remote Operations Devices Ideas

Use this portal to submit your innovative ideas to make Geo SCADA Expert and Devices such as SCADAPack, Trio and Realflo of greater value to you and to the SCADA & Telemetry community. Every idea will be individually reviewed by our team for merit and will be marked Under Consideration.
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
  • Remote Operations
  • Geo SCADA and Remote Operations Devices Ideas
  • Advanced Modbus driver optimization
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
  • Alphabetical
  • SCADA 2
  • ViewX 2
  • Mimics 2
  • SCADAPack 2
  • Scripting 1
  • Virtual ViewX 1
  • Geo SCADA Expert 1
  • Efficiency 1
  • Configuration management 1
  • Modbus to WiStar 1
Idea Statuses
  • Submitted 14
  • Under consideration 139
  • Accepted 1
  • Declined 5
  • Partially delivered 0
  • Delivered 3
  • Abandoned 0
Related Products
Thumbnail of EcoStruxure™ Geo SCADA Expert
Schneider Electric
EcoStruxure™ Geo SCADA Expert
118
Thumbnail of SCADAPack 57x
Schneider Electric
SCADAPack 57x
2
Thumbnail of Accutech
Schneider Electric
Accutech
1
Load more
Completed Ideas
  • Tag Bit addressing for the EtherNet/IP driver

  • Geo SCADA Expert as OPC-UA server

  • OPC-UA Driver

  • API driver

  • Accutech Modbus Master gateway to read Modbus devices and incorporate into WiStar net

View All
Top Liked Authors
User Likes Count
GeoffChisholm
GeoffChisholm
2
View All

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
0 Likes

Advanced Modbus driver optimization

Status: Under consideration Submitted by support402 Explorer on ‎2023-03-06 01:50 PM
2 Comments (2 New)

This feature request comes from a customer via bFO # 98925769 and # 98053984 as well as JIRA CSUP-13309.

The initial request was to optimize the driver to poll outstations as fast as possible (as they used to use a competitors SCADA system which performed that way).  After discussing the pros/cons of that type of architecture, this customer chose to set up a separate channel for "Fast Scan" polling.  Below are comments from the customer regarding this operation.

 

Switching Outstation to a separate “Fast Scan” channel and allowing IP100 to handle flow of communications helped, but did not completely resolve issues. When switching outstation back to “Normal Scan” channel it does a restart sequence similar to what a refresh does. SE development team should look at improving  how Adv modbus driver handles communication flow and implement a better way of promote / refresh outstations. Outstation retrieval intervals is a great way to optimize points that don’t need to be poll often, but there should also be away to set poll interval to poll data fast as possible and still allow promote scan to work as it was intended to!

Tags (5)
  • Find more ideas tagged with:
  • english
  • scada
  • SCADA app
  • SCADA software
  • SCADA tutorial
Comment

Link copied. Please paste this link to share this article on your social media post.

  • Back to Idea Exchange
  • Previous
  • Next
2 Comments
AndrewScott
AndrewScott
Leader
‎2023-03-09 06:50 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2023-03-09 06:50 AM

To poll a Modbus point as fast as possible set it's Retrieval Interval to Continuous.

Points Used on Generic Modbus Controllers \ Configure Common Point Properties 

 

Whilst there isn't a specific promoted retrieval interval for continuous, setting the interval to a very small value (e.g. 1ms) will achieve the same effect.

Configuring a Generic Modbus Controller \ Define the Data Retrieval Intervals 

This allows points to be promoted from their normal retrieval interval to 'continuous' using any type of promoted scanning (manual promotion, promote on display, promote after control).

Temporarily Increasing the Scan Rate 

 

 

When using two channels for "Normal Scan" and "Fast Scan" how are they switching between channels? Are they using a switched / shared outstation set and switching lines, or are they reconfiguring the outstation (or set) to a different channel? All of these will stop and restart comms with the outstation when switching. Making configuration changes for operational reasons should be avoided as its not efficient.

sbeadle
sbeadle Champion
Champion
‎2024-12-20 05:30 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2024-12-20 05:30 AM
Status changed to: Under consideration

Thank you

Comment
Preview Exit Preview

never-displayed

Hint:
@ links to members, content
 
  • Back to Idea Exchange
  • Previous
  • Next
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.