Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Using more than 2GB Memory in Windows

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Using more than 2GB Memory in Windows
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 11:49 AM
0 Likes
0
2241
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
‎2021-06-09 11:49 AM

Using more than 2GB Memory in Windows

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 08:49 PM

📖 Home  Back  

 

32-bit versions of Windows are rare these days, this article is still here in case you are running old operating systems. On 64-bit versions of Windows, 32-bit processes can address the full 4GB of memory

 

Windows XP and 2003 32-bit operating systems can only address 4GB of RAM in total. By default, 2GB is reserved for user processes and 2GB for kernel usage. Normally, when a process reaches 2GB of memory used (2048MB, or roughly that number), the next request for memory will be refused. This will have undesirable effects in ClearSCADA leading to unexplained events such as server failures. In this scenario, an exceptions log will not be created as this process requires memory that is not available.

Windows (XP, 2003) can be set to change the 2GB user limit to 3GB, at the sacrifice of available kernel memory (2GB -> 1GB).

To do this, modify the boot.ini file (in the root directory of C drive) to have a /3GB switch for the operating system start up line (see http://support.microsoft.com/kb/833721) and reboot. Note that Windows hides the boot.ini file by default as a protected system files. This setting can be changed in the Folder Options of Windows Explorer.

An example file is:

[boot loader]
timeout=30default=multi(0)disk(0)rdisk(0)partition(1)\WINDOWS[operating systems] multi(0)disk(0)rdisk(0)partition(1)\WINDOWS="Windows Server 2003, Enterprise" /noexecute=optout /fastdetect /3GB


The 32-bit process also needs to have a special flag set in it that allows it to use this feature of Windows. This feature is available from ClearSCADA 2005 R0 onwards. To view the amount of memory available to the ClearSCADA server, view the "Available Virtual Memory" setting on the Info tab of the ClearSCADA Server Status dialog.

In rare cases, networking problems have been seen on systems with the /3GB set. This has been seen as unexplained network-connected driver channels and SNMP points failing within ClearSCADA, and seems to be due to less kernel memory being available to Windows (1GB instead of 2GB). Boot.ini can be modified again to add the "/Userva=3030" switch, which allows more memory for Windows to assign to network resources, relieving the problem.

See http://support.microsoft.com/?kbid=810371 for more information.

This would make the above line in the file:

multi(0)disk(0)rdisk(0)partition(1)\WINDOWS="Windows Server 2003, Enterprise" /noexecute=optout /fastdetect /3GB /Userva=3030


Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.