Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Triggering Logic On Input Processed

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Triggering Logic On Input Processed
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 03:02 PM
0 Likes
0
1095
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
‎2021-06-09 03:02 PM

Triggering Logic On Input Processed

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 10, 2021 12:02 AM

📖 Home  Back  
On Input Processed can be used to trigger the execution of a Logic program whenever one of the inputs in processed. On Input Processed can be used for the following data types:
  • Digital and Analogue Points

  • Digital and Analogue Variables

  • Accumulators


Reference to configuration fields (units, format, multiplier for example) will not trigger an Input Processed events. For the program to execute, it must be some sort of state change, such as a new value from the outstation.

You may see the following occur if your On Input Processed logic program is not configured correctly.


Program Will Not Run


Your program may not run if you use the wrong type of object, or property as the input.  This is because the program triggers when an input is processed, not when it changes.

If you want a logic program to trigger off an object property that is not processed e.g. the value of a parameter, then you should use 'On Interval', set the program up to run periodically and select 'Input Change Detection'. This means that the program will check your inputs according to the configured execution Interval and only run if the inputs have changed.

If the trigger you require is not one of the program inputs then you can use the 'Trigger' field. This will check for changes in your 'Trigger' according to the configured execution Interval and only execute if the 'Trigger' has changed.

If you have reference to a configuration field in your logic program (units, format, multiplier for example), then when you change the property value and save the form, it will not cause the logic program to execute.  For the program to execute, it must be some sort of state change, such as a new value from the outstation.


Errors when Writing to a Point Used as Input


If you are trying to read from the point and also write to it, it will not be used as a trigger to run the logic program.

For it to be used as a trigger it has to be used in a read-only way (so you can declare the variable as %I). If the variable was written to and also acting as a trigger, program would go into an infinite loop, because as each execution cycle ended, the value would be written to and so the logic would trigger again and repeat the cycle.  ClearSCADA will flag a compile error if you write to an input in the program, and have no other inputs for the program.  If there are other inputs, then the input being written to will not be used as an input for the On Input Processed calculations.


Program Runs Multiple Times


If you have two inputs to the program, each of which changed at the same time, the logic program will be executed twice. That is, once for each point update. If you have many inputs from the same object, all of which changed in the point update, the logic program will only execute once.

Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.