Outstation Point Statistics

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Outstation Point Statistics
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Using Python with Geo SCADA - Introduction
  • Sparkplug Quality Mapping
  • Geo SCADA 2025 Upgrade Strategy
  • Geo SCADA 2025 Known Issues
  • Geo SCADA 2025 Upgrade Notes
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 12:51 PM
0 Likes
0
1141
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
‎2021-06-09 12:51 PM

Outstation Point Statistics

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 09:51 PM

📖 Home  Back  
The database tables CAdvOutstation and CPointSource each contain five database fields to monitor the processing load caused by each outstation / point source. These statistics are intended to provide an indication of the load on the system from telemetry, and identify which outstations / point sources are creating the greatest load.

The five fields for advanced driver outstations (such as SCADAPack Modbus and DNP3) are as follows:

 Table Name Field Name Description
 CAdvOutstation PointProcessCount Number of updates for outstation's points since last reset.
 CAdvOutstation PointHistoricCount Number of historic updates for outstation's points since last reset.
 CAdvOutstation PointAlarmCount Number of alarm updates for outstation's points since last reset.
 CAdvOutstation PointEventCount Number of events for outstation's points since last reset.
 CAdvOutstation PointCountTime Time from which point statistics are being measured.


The five fields for simple driver point sources (such as Modbus and OPC) are as follows:

 Table Name Field Name Description
 CPointSource PointProcessCount Number of updates for point source's points since last reset.
 CPointSource PointHistoricCount Number of historic updates for point source's points since last reset.
 CPointSource PointAlarmCount Number of alarms updates for point source's points since last reset.
 CPointSource PointEventCount Number of events for point source's points since last reset.
 CPointSource PointCountTime Time from which point statistics are being measured.


All of these fields are updated by the point processor when processing updates for the points on the outstation or point source (i.e. data retrieved from the outstation or point source, along with master station overrides).

  • If a point update results in a state change which causes alarm(s) to be raised and/or cleared then the PointAlarmCount is incremented once for each alarm raised or cleared.

  • If a point update results in a significant change and/or state change and is configured to log an event then the PointEventCount is incremented for each event logged. It is also incremented for any events logged relating to alarms being raised and/or cleared as a result of a state change.

  • If a point update is stored in the historian then the PointHistoricCount is incremented.

  • Every point update causes the PointProcessCount to be incremented.


Also, the database table CDBPoint contains two database fields to monitor the processing load caused by each individual point. The two fields are as follows;

 Table Name Field Name Description
 CDBPoint ProcessCount Number of times that the point has been updated, since last reset.
 CDBPoint ProcessCountTime Time from which point statistics are being measured.


Every point update causes the ProcessCount to be incremented, including hand control of internal points.


The method ResetPointStatistics in the CAdvOutstation and CPointSource tables can be used to clear the outstation point statistics and/or all the individial point statistics and initialise the PointCountTime and ProcessCountTime fields to the current time. It is recommended that the statistics are reset periodically, such as once a week.

The method ResetProcessCount in the CDBPoint table can be used to clear the statistics for a single point and initiailise the ProcessCountTime to the current time.


Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.