Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Multiple Parameters in an SQL Command in Logic

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Multiple Parameters in an SQL Command in Logic
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 12:40 PM
0 Likes
0
3445
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
‎2021-06-09 12:40 PM

Multiple Parameters in an SQL Command in Logic

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 09:40 PM

📖 Home  Back  
To enter multiple parameters in an SQL command within a Logic program, you need to use the ? character to represent the value of each parameter, and the WITH_PARAMS keyword to define the parameters.

The order of the parameters that you define after the WITH_PARAMS keyword corresponds to the order of the ? characters defined in the SQL query. You can repeat the parameters so that the same parameter can be used multiple times in the SQL.

When entering multiple parameters in an SQL command in Logic, you need to use the ? character to represent each parameter value in the query. The WITH_PARAMS keyword must be used in the RESULTSET and each parameter listed after the WITH_PARAMS keyword must correspond to the name of one of the Logic program's VAR inputs. You should separate the parameters after the WITH_PARAMS keyword with commas.

Example

In this example of an ST Program, the parameters for the SQL query are defined as VAR_INPUTs with the names objName and objFullScale. In the SQL query, the ? character is used to represent the parameters. Note that DATABASE_OBJECT is used to define the database table (in this case, CPointAlg) and the type of value for the properties defined in the SQL query (Name and FullScale).

TYPE
Point: DATABASE_OBJECT (CPointAlg)
Name:STRING;
FullScale: LREAL;
END_DATABASE_OBJECT;
END_TYPE

PROGRAM NameAndFullScale
VAR_INPUT
objName : STRING;
objFullScale: LREAL;
END_VAR
VAR
objList AT %S(SELECT Id, Name, FullScale FROM CPointAlg WHERE Name LIKE ? || '%' AND FullScale > ?) : RESULTSET OF Point WITH_PARAMS objName, objFullScale;
END_VAR;

(* Insert program code here *)

END_PROGRAM


So, the SQL query in the ST Program will return the Id, Name, and FullScale values from the CPointAlg database table. It will only return the values for those items that have a Name value that is like the value of the first parameter followed by any amount of characters and has a FullScale value that is greater than the value of the second parameter. The first parameter is the objName parameter as this is the first parameter listed after the WITH_PARAMS keyword. The objFullScale parameter is the second parameter as it is listed second after the WITH_PARAMS keyword. So in the SQL query, the first ? character corresponds to the objName parameter and the second ? character corresponds to the objFullScale parameter.

If the SQL query was to contain an additional ? character, an additional parameter would be required in the list of parameters after the WITH_PARAMS keyword. The additional parameter in the list could be a new parameter or could be one of the existing parameters used again, for example, it could be another use of the objFullScale parameter.
You can use a DATE_AND_TIME as a parameter, however unlike normally in the SQL you leave out the TIMESTAMP keyword as it is automatically dealt with.


Go: Home Back

Labels:
  • database

  • IEC 61131-3 Logic

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.