Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Communications State - Failed (IO Timeout)

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Communications State - Failed (IO Timeout)
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 11:42 AM
0 Likes
0
2200
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
‎2021-06-09 11:42 AM

Communications State - Failed (IO Timeout)

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 08:42 PM

📖 Home  Back  
The designers of ClearSCADA realized that in some cases it is advantageous to declare that a channel is failed, well before communications has failed to all the outstations. An example of this is for a channel with 50 outstations attached to it, and communications has been unsuccessful to 25 of them. In this scenario it is likely that there is a technical problem causing this channel to fail as it is unlikely that 25 outstations are out of service. Instead of continuing to check the availability of the other 25 outstations, it is reasonable to declare that the channel has failed and raise an alarm. Why wait for the other 25 outstations to fail before setting the alarm and telling the operator?

This behaviour of ClearSCADA is defined in the server configuration on the Global parameters -> Channel page. The relevant settings are:
  • maximum number of consecutive failed reads timeouts

  • maximum number of consecutive failed writes timeouts


These settings are set, by default, to 20 and 20 respectively. This typically allows for a small number (1-2 depending on the protocol and channel configurations) of outstations to fail before the channel is failed with the (I/O timeout) alarm.

In systems where there are large numbers of outstations on one channel, these settings will not be suitable. Having the settings too low will cause a channel to be failed with I/O timeout if there is a communication failure to a very small percentage of the outstations on the channel. It is possible that 3 outstations are being serviced at once, for example, and the other 47 outstations are still available. It is recommended that the maximum number of consecutive failed read/writes be increased to a point where a "reasonable" number of outstations that are offline do not cause the channel to be failed.

It is also worth noting the behaviour of a channel with only one outstation. It is unlikely to ever fail due to the server settings for maximum number of consecutive failed reads or writes. What will normally happen is the outstation will be declared as failed, and therefore the channel will stop trying to poll the only outstation, except for the re-establishment polls. What this means is that the outstation will alarm but the channel will not so it is important for the user to understand the importance of both channel and outstation alarms when troubleshooting.

When using switched outstation sets, it is especially important that the channel does not fail due to the max number settings as the switched outstation set will automatically switch to the backup channel when the server settings are reached and the switched outstation set will not follow its own setting for "Switch after X outstations have failed". This may cause confusing behaviour as the channel and the switched outstation set settings work against each other.

It is recommended that the server maximum number settings are increased to a point where the switched outstation set "switch after ..." setting has already acted.

Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.