Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354357posts

LUFP7 Profibus DP / Modbus Gateway Software

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

Solved
swil
Commander
Commander
0 Likes
1
318

LUFP7 Profibus DP / Modbus Gateway Software

I'd like to map modbus RTU addresses to Profibus DP using a LUFP7 Gateway.

1. Can I map custom modbus-RS485 registers to custom Profibus addresses with LUFP7?

2. Where can ABC-LUFP Config Tool programming software be downloaded from, and is it compatible with modern operating systems? (2009 documentation referred to)

 

Tags (1)

Accepted Solutions
Daniel_Borle
Commander Commander
Commander

Re: LUFP7 Profibus DP / Modbus Gateway Software

Hi Scott,
The LUFP7 is a very old device (I'm even not sure whether it is still available or not) and I don't think that the software (ABC-LUF config tool) will run on new OS (maybe in compatibility mode). For this I normally run it on a Windows 7/XP VM.

It is possible to use it for custom devices that are communicating over RS485 with Modbus-RTU (see attached document that we created many years ago).

But you must be aware that one is very limited with this gateway: 128 16-bit registers max. in total for all connected slaves and each request has to be programmed. You must also be very careful with timings

Just a suggestion from me: Use Anybus X-Gateway instead. The advantage is, that it can be "programmed" over integrated web pages and if applicable in your system, it can also support Modbus-TCP with Profibus DP which means, that you can connect your devices to a simple gateway like the Link150 and communicate in parallel with the Anybus X-Gateway to the devices over the Link150. So your system stays open that the connected devices can communicate with a Modbus system like PME on one side and to a Profibus system on the other side (which is not the case with a LUFP7 where you will end on Profibus DP). Here is a link to the HMS page where you can select the gateway with the networks/protocols (1 and 2) that shall be supported:

https://www.anybus.com/products/gateway-index

BR

Daniel

 

See Answer In Context

Attachments
Tags (1)
1 Reply 1
Daniel_Borle
Commander Commander
Commander

Re: LUFP7 Profibus DP / Modbus Gateway Software

Hi Scott,
The LUFP7 is a very old device (I'm even not sure whether it is still available or not) and I don't think that the software (ABC-LUF config tool) will run on new OS (maybe in compatibility mode). For this I normally run it on a Windows 7/XP VM.

It is possible to use it for custom devices that are communicating over RS485 with Modbus-RTU (see attached document that we created many years ago).

But you must be aware that one is very limited with this gateway: 128 16-bit registers max. in total for all connected slaves and each request has to be programmed. You must also be very careful with timings

Just a suggestion from me: Use Anybus X-Gateway instead. The advantage is, that it can be "programmed" over integrated web pages and if applicable in your system, it can also support Modbus-TCP with Profibus DP which means, that you can connect your devices to a simple gateway like the Link150 and communicate in parallel with the Anybus X-Gateway to the devices over the Link150. So your system stays open that the connected devices can communicate with a Modbus system like PME on one side and to a Profibus system on the other side (which is not the case with a LUFP7 where you will end on Profibus DP). Here is a link to the HMS page where you can select the gateway with the networks/protocols (1 and 2) that shall be supported:

https://www.anybus.com/products/gateway-index

BR

Daniel

 

Attachments
Tags (1)