Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Minor Update with Bug Fixes:
* [artf147374] : Custom Models - The custom device types units selection is not honored
* [artf147373] : Custom Models - The use of a fractional "Factor" is not properly supported in the Com'X 510 for all register formats
* [artf148188] : Custom Models - Function code x03 is used when x04 is specified
* [artf147384] : Custom Models - Overlapping frames causes topics to go offline
* [artf148273] : artf148273 : Energy Dashboards - Date Picker in Dashboards Does Not Honor The Date Time Format
Link copied. Please paste this link to share this article on your social media post.
Hello,
I did the upgrade of the Com'X510 but now it is impossible to acces the device. The upgrade went up to 98% up to rebooting the device. After that it was impossible to acces the device webpage. No reply to a ping of the programmed IP, no discovering in the windows exporer network...
I did the factory with power off and pushing the two buttons(backup+wifi) and repower... still no communication of detection in the windows network devices...
I did also the update via USB but still same problem...
Any other sugestions?
Link copied. Please paste this link to share this article on your social media post.
Hello Koen,
I'm sorry to hear that you are having this issue. How long has it been since the box rebooted? Are you seeing a green light by the word "Power" on the front of the box?
Robert Jennings - Have you seen this before?
James
Link copied. Please paste this link to share this article on your social media post.
Hello James,
The device is back online with firmware 1.1.45. I disconnected the device for about 1h and did some tests on an other 510. After reconnecting the device and waiting for green led i could reconnect via the port2 via the 10.25.1.1 addres...
Maybe I didn't wait long enough after the reboot...
In the log I can not find any errors...
Link copied. Please paste this link to share this article on your social media post.
Hello,
Is it normal that negative values are not shown in the historical trending? Is this a parameter that we can set?
Kind regrads,
Koen
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.