Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84244members
353343posts

EGX300 Firmware v4.350.zip

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

JamesJeanette
Commander Commander
Commander

EGX300 Firmware v4.350.zip

 

Downloads

 

EGX300 Firmware & Disk Image Update

 

Version 4.350 firmware provides:

·          Ability to append EGX300 MAC Address to Device Log Export file for name uniqueness

 

Version 4.350 Disk Update provides:

Device Log Export:

·          Added checkbox to allow user append the EGX300 MAC Address to the log file name to ensure the file name is unique.

Device Support:

·          Added the following devices

o    PM5100/PM5300 Series Meters

o    EM4800

o    PM5560

o    Conext TL

·          Added support for Inputs for the following devices

o    iEM3155

o    iEM3255

o    PM3255

·          Fixed scaling issue for Acti9 Smartlink logging

·          Fixed issue with MCM Real Power not being displayed

·          Fixed issue with PM3150/3155/3250/3255 not displaying Power in Real Time Trend

 

*Upgrading to version 4.350 requires new firmware to be downloaded to the EGX followed by the egx04350.upd Disk Image. 

 

Firmware Download Instructions for EGX300

Currently Running Firmware Version 3.7xx

 

Updating to version 4.350 from version 3.7xx requires all data log files to be converted internally.  This conversion will be executed at the first boot after the download.  While converting the data log files, browsing of the EGX will be limited to a page displaying the status of the conversion until conversion is complete.  Depending on the size and number of the data log files, this process may take several minutes. 

 

Before downloading the firmware, logging must be disabled.  It is recommended the user save all data log files to external storage before downloading.  Refer to the EGX300 User’s Guide for instructions on how to disable logging and remove data log files. 

 

1.     Disable Logging.

2.     Save data log files to external storage (optional but recommended).

 

3.     Remove data log files (optional but recommended).

4.     Transfer the version 4.350 firmware file (egx04300.bin) to your computer.

 

5.     Use FTP to copy the “egx04300.bin” file from your computer to the EGX300.  The status LED will flash rapidly while the firmware is being programmed.  Do not remove power during this time.  Once the download is complete the EGX will automatically reboot.  Refer to the EGX300 User’s Guide if you need more information.

 

6.     Allow the EGX to reboot after the firmware file transfer, then browse the EGX300 Diagnostic Statistics page and confirm V4.350 is displayed as the Firmware Version in the Gateway Information section. 

 

7.     After confirming the firmware has been updated apply the V4.350 Disk Update.


 

Firmware Download Instructions for EGX300

Currently Running Firmware Version 3.800 or Greater

 

Before downloading the v4.350 firmware, it is recommended to disable logging and to save all data log files to external storage.  Refer to the EGX300 User’s Guide for instructions on how to disable logging and remove data log files. 

 

1.     Disable Logging.

2.     Save data log files to external storage (optional but recommended).

 

3.     Remove data log files (optional but recommended).

4.     Transfer the version 4.350 firmware file (egx04350.bin) to your computer.

 

5.     Use FTP to copy the “egx04350.bin” file from your computer to the EGX.  The status LED will flash rapidly while the firmware is being programmed.  Do not remove power during this time.  Once the download is complete, the EGX will automatically reboot.  Refer to the EGX300 User’s Guide if you need more information.

 

6.     Allow the EGX to reboot after the firmware file transfer then browse the EGX300 Diagnostic Statistics page and confirm 4.350 is displayed as the Firmware Version in the Gateway Information section. 

 

7.     After confirming the firmware has been updated apply the V4.350 Disk Update.

Attachments