Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Disk Update version V4.210 is released in support of V4.200 firmware. This release replaces Disk Update Version V4.200.
Link copied. Please paste this link to share this article on your social media post.
Downloads
EGX300 Firmware & Disk Image Update
Version 4.200 firmware provides: · Improved Custom Device Type Generator support · CO2 and Irradiance topic support
Version 4.210 Disk Update provides: · All improvements provided by V4.200 · Corrected Compact NSX and PowerPact Date/Time display · Support for the following devices. o EM1210 o EM1250 o EM1251 o PM3250 o PM3255
Previous Disk Version V4.200 added support the following devices: · iEM3150 · iEM3255 · iEM3250 · iEM3255 · Acti 9 SmartLink
*Upgrading to version 4.200 requires new firmware to be downloaded to the EGX followed by the egx04210.upd ‘patch’ to the suite of files located on the EGX300 flash disk.
|
Firmware Download Instructions for EGX300 Currently Running Firmware Version 3.7xx
Updating to version 4.200 from version 3.7xx requires all data log files to be converted internally. This conversion will be executed at the first boot after the download. While converting the data log files, browsing of the EGX will be limited to a page displaying the status of the conversion until conversion is complete. Depending on the size and number of the data log files this process may take several minutes.
Before downloading the firmware logging must be disabled. It is recommended the user save all data log files to external storage before downloading. Refer to the EGX300 User’s Guide for instructions on how to disable logging and remove data log files.
1. Disable Logging.
2. Save data log files to external storage (optional but recommended).
3. Remove data log files (optional but recommended).
4. Transfer the version 4.200 firmware file (egx04200.bin) to your computer.
5. Use FTP to copy the “egx04200.bin” file from your computer to the EGX300. The status LED will flash rapidly while the firmware is being programmed. Do not remove power during this time. Once the download is complete the EGX will automatically reboot. Refer to the EGX300 User’s Guide if you need more information.
6. Allow the EGX to reboot after the firmware file transfer, then browse the EGX300 Diagnostic Statistics page and confirm V4.200 is displayed as the Firmware Version in the Gateway Information section.
7. After confirming the firmware has been updated apply the V4.210 Disk Update (patch).
|
Firmware Download Instructions for EGX300 Currently Running Firmware Version 3.800 or Greater
Before downloading the v4.200 firmware it is recommended to disable logging and to save all data log files to external storage. Refer to the EGX300 User’s Guide for instructions on how to disable logging and remove data log files.
1. Disable Logging.
2. Save data log files to external storage (optional but recommended).
3. Remove data log files (optional but recommended).
4. Transfer the version 4.200 firmware file (egx04200.bin) to your computer.
5. Use FTP to copy the “egx04200.bin” file from your computer to the EGX. The status LED will flash rapidly while the firmware is being programmed. Do not remove power during this time. Once the download is complete the EGX will automatically reboot. Refer to the EGX300 User’s Guide if you need more information.
6. Allow the EGX to reboot after the firmware file transfer then browse the EGX300 Diagnostic Statistics page and confirm 4.200 is displayed as the Firmware Version in the Gateway Information section.
7. After confirming the firmware has been updated apply the V4.210 Disk Update (patch).
|
Download Instructions for EGX300 4.210 Disk Update (patch)
Version 4.200 firmware requires updates to support files within the EGX300. Version 4.210 Disk Update file will apply these updates.
1. Disable Logging.
2. Transfer the version 4.210 Disk Update file (egx04210.upd) to your computer.
3. Use FTP to copy the “egx04210.upd” file from your computer to the EGX. The status LED will flash rapidly while the disk is being updated. Do not remove power during this time. Once the download is complete the EGX300 will automatically reboot.
4. Allow the EGX300 to reboot after the files have been updated. Browse the Maintenance page in the EGX and verify that there is Entry Detail for “applied patch 2012-06-14-14-34”.
Note: Many of the files in the update are web pages that may be currently cached in your browser. It may be necessary to force your browser to reload a page using <CTRL> + <F5> before the new page is displayed. In some cases you may need to flush your browser’s cache of web pages.
|
Link copied. Please paste this link to share this article on your social media post.
Hi James,
Do you know when version 4.3 is to be released?
Thanks
Colin
Link copied. Please paste this link to share this article on your social media post.
EGX300 Firmware Version 4.300 is complete and I will be uploading to the various sites, including here this week. Look for it very soon!
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.