Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Hi
Regarding PowerTag A9MEM1560 and A9MEM1570 I can´t see is possible to get measurement readings i Com´X510 with latest firmware v 5.2.0.
Gateway is SI-D
Get measurements in SI-D and Ecoreach
This PowerTag A9MEM1560 and A9MEM1570 is not able to select in meny Device Settings-Modbus Serial.
Tryed to use 1520 that is selectable but not able to get measurements readings.
So if not supported in this Firmware version v 5.2.0 will this PowerTags be supported in the next version ?
When is the release date ?
Best Regards
Anders
Link copied. Please paste this link to share this article on your social media post.
The iEM2050 and iEM2055 will be available in firmware version 7.0.
Thanks,
Randi
Link copied. Please paste this link to share this article on your social media post.
Hi Anders,
You are correct. The Com'X does not support the PowerTag 1560 and 1570 with the current released firmware, 5.2.0.
The Com'X will provide support for the PowerTag 1560 and 1570 starting with version 6.0. I believe this version will be available in a few months. The code will be "frozen" this week and then it will be subject to regression and system testing. After these tests are complete, the firmware will be released to the public.
We apologize for any inconvenience this has caused in the meantime.
Best regards,
Randi
Link copied. Please paste this link to share this article on your social media post.
Thanks for the info, no problem. Will inform customers.
How about the new 1-phase energy meter A9MEM2050, A9MEM2055 ? FW 6.0 ?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Hi
Is there any more timeline for FW 6.0 ?. We have project that is an ongoing discussion with customer if we can give some kind of answer.
BR Anders
Link copied. Please paste this link to share this article on your social media post.
Hi Anders,
Com'X Version 6.0.x will be available mid-May.
I hope this helps.
Best regards,
Randi
Link copied. Please paste this link to share this article on your social media post.
Hi
It helps a lot, many thanks
BR Anders
Link copied. Please paste this link to share this article on your social media post.
Hi @Randi_Dolan
For information (with v5.2) if I add Powertag 1540 and 1541 directly with Zigbee Dongle :
Thanks !
Romain
Link copied. Please paste this link to share this article on your social media post.
Hi Romain,
Direct support for the PowerTag devices has been postponed in the Com'X. We currently do not have plans to directly support the PowerTag. If you are getting readings in the Measurement table, it's just luck 🙂
Best regards,
Randi
Link copied. Please paste this link to share this article on your social media post.
Hi
Any news about the release FW6.0 ?
BR/Anders
Link copied. Please paste this link to share this article on your social media post.
Hello Randi,
OK 🙂
FYI my architecture below. As you see, there are some values for Powertag in ndirect Zigbee.
But I cannot have Gauges or Basic values in the Monitoring tab.
Do you plan to integrate the Powertag Link and Powertag Link HD in the FW 6.0 ?
Thanks !
Romain
Link copied. Please paste this link to share this article on your social media post.
Hi Anders,
The firmware is undergoing some additional testing and should be available by the end of July.
Best regards,
Randi
Link copied. Please paste this link to share this article on your social media post.
Hi Romain,
The PowerTag and PowerTag Link HD will not be a part of the Com'X 6.0 firmware.
Best regards,
Randi
Link copied. Please paste this link to share this article on your social media post.
Hello.
How did you add PowerTags to Com'X?
I have Com'X 510 with ZigBee dongle.
Thanks.
Link copied. Please paste this link to share this article on your social media post.
Hello
Com´X510 need to have FW 6.0.4. PowerTag is connected (ZigBee) to SI-D what is communicating with Com´X510. SI-D is a device in Ethernet meny below Device Settings.
BR/Anders
Link copied. Please paste this link to share this article on your social media post.
Hello @Boris_Horvat
PowerTag Energy Sensors are not directly integrated in the FW 6.0.4.
It means that you cannot connect them to the Zigbee Dongle of the Com'X. You can try : PowerTag will be detected but you will have a lot of inconsistencies on the data displayed by the Com'X interface.
Currently you need to pair your PowerTag Energy Sensor with a gateway like Smartlink SI B, PowerTag Link SD or PowerTag Link HD (Smartlink SI D is not recommended for new business).
After that, you need to :
Regards,
Romain
Link copied. Please paste this link to share this article on your social media post.
I thought you connect PowerTag directly to Com'X.
I have also Smartlink gateway and it works.
But I wanted to connect them directly with ZigBee dongle.
What for can I use ZigBee dongle on Com'X?
Link copied. Please paste this link to share this article on your social media post.
Hi,
With FW 6.0.4 you can directly connect the CL110 and TH110 Wireless Temperature sensors.
With older FW release you can also connect the EM4300 Energy Meter.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.