Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Hello,
I am logging flow temperature, return temperature, energy and volume flow to a Com'X200. This data is then published to a server via FTP. Logging is enabled in "Commissioning" as well as in "Device Settings", and I can see the device and all it's values under "Measurements Table". See screenshots:
However, when I check the published .csv file, see attached, volume flow "Water_Volume_Flow_Rate_(m^3/h) is not there. I have tried restarting the Com'X as well as leaving it to log over night before publishing any data. The firmware is up to date.
Any suggestions as to why?
Thanks!!
Link copied. Please paste this link to share this article on your social media post.
Dear Schneider Tech Support Folk,
This is now logged as a case (no 42111660) and which I believe has been escalated to L3 in Victoria. I have not received any response other than saying the files cannot be opened.
I am due to hand the system over to my client on Monday, and they will be exceptionally cranky if I tell them one of their Com'Xs are not logging, as well as being rather embarrassed...
Please assist.
Thank you.
Posted: 2017-09-19 07:34 AM
Link copied. Please paste this link to share this article on your social media post.
Hi,
Can you please do a Manual Export of the data and then save the diagnostic logs for us? It will aid us in this investigation.
Best Regards,
Colton
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.