New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
COM'X 510 - No Modbus TCP Device Data
Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
2023-03-0103:06 PM
COM'X 510 - No Modbus TCP Device Data
Experiencing an issue where a COM'X is no longer able to load data from PM8000s due to "A communication error has occurred". The COM'X is showing TCP connection timeouts for each device. Restarting the COM'X and increasing timeout parameters has not changed anything.
Firmware:
COMX510 - 6.5.4
PM8000 - 3.1.0
PAS600L - 1.5.1
Customer has the following project architecture:
- LX40_1: 2x PM8000 (Ethernet daisy chain)
- LX40_2: 1x COM'X 510
- LX40_3: 1x PAS600L
- LX40_4: 1x PAS600L
The intention is for the COM'X 510 to serve as the principal energy server where all other WAGES (collected by PAS600Ls) and electrical data (PM8000s) are displayed and logged. Each LX40 router is equipped with a public static IP address (Telus SIM cards) and the communication on the Telus network works properly. The public static IPs have changed over the course of the project due to having to replace SIM cards, however the COM'X data was verified successfully before and after these changes.
LX40_1 uses the following port forwarding rules, and I can successfully connect to the meters webpages using 9444 and 9445:
<PublicIP>.9502 --> <PM800_1>.502
<PublicIP>.9444 --> <PM800_1>.443
<PublicIP>.9503 --> <PM800_2>.502
<PublicIP>.9445 --> <PM800_2>.443
Similar port forwarding rules are used for the other LX40s, with the same issue that HTTPS data is working but Modbus is not. As a test, I checked whether LX40_3 could read Modbus data from the PM8000s connected to LX40_1 or PAS600L connected to LX40_4, however getting the same issue of connection timeout.
Please see COMX diagnostics and configuration files attached and also screenshots attached of Modbus parameters of COM'X, PM8000 and PAS600L. Any troubleshooting advice would be appreciated.