Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Hi,
I recently tried to get the Com'X510 / 200 to publish via Gmail / Hotmail and it seemed to me that there is no TLS encryption implementation for the Com'X gateways, which means it can't use these extremely useful public SMTP relays.
I had to use a third party TLS certificate proxy to get it to work (effectively adds TLS encryption to the unencrypted connection that the Com'X uses), however this implementation requires a computer be running with the proxy always running, which is not always possible.
Regards,
Steven Yan
Posted: 2017-03-20 03:57 AM
Link copied. Please paste this link to share this article on your social media post.
Hi,
Yes you are right, for the moment ComX only support unencrypted SMTP connection, publishes data without TLS encryption.
I tested several time com'x publication using google SMTP server "aspmx.l.google.com", it works !
Port 25, TLS not required Dynamic IPs allowed Mail can only be sent to Gmail or Google Apps users, it's mean that "from email:" and "to email:" most be google account, smtp restricted only for google users. G Suite SMTP settings to send mail from a printer, scanner, or app - G Suite Administrator Help
Link copied. Please paste this link to share this article on your social media post.
Thanks Lazaro, I did try that, but I didn't use both "To" and "From" addresses as gmail (one of them was a Schneider) and so it didn't work.
Link copied. Please paste this link to share this article on your social media post.
Unfortunately the Com'X510 says it is successful, however no emails turn up. I think it must be hitting some filter that gmail is running and rejecting it.
Posted: 2017-03-22 07:20 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Steven,
We are currently implementing this feature (SMTP Publication over TLS). Bobbie Meredith can comment further as to when it will be available.
Best,
Colton
Link copied. Please paste this link to share this article on your social media post.
Can we expect it in V4 f/w?
Posted: 2017-09-06 05:25 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Grant,
Yes, SMTP Publication (and Email on Event) will be available in v4.0 over both TLS and STARTLS.
Best Regards,
Colton
Posted: 2017-09-27 07:04 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Experts,
News about TLS implementation?
BR
Bryan
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.