Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Animation of double signal switches in IEC61850 Power Operation

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • Animation of double signal switches in IEC61850 Power Operation
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
117
Guillaume_Evrard
Captain Guillaume_Evrard Captain
59
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
Schneider Electric
EcoStruxure™ Power Operation

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Gateways and Energy Servers
Start a Topic
Solved
sebastian.contreras
Crewman sebastian.contreras
Crewman

Posted: ‎2023-01-12 11:34 AM . Last Modified: ‎2023-01-12 11:40 AM

0 Likes
4
1758
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
‎2023-01-12 11:34 AM

Animation of double signal switches in IEC61850 Power Operation

Hello everyone!

 

Please help me on the following topic!

 

We need to animate an HMI, which refers to a substation, here we have to animate the switches with double points, these points are given to me by the CID file, specifically from the SCSWI1.Pos.StVal node (IEC61850 node), this node has 4 states : 0, 1, 2 and 3.
But when it comes to animating the object, it only takes states 0 and 1, therefore, it makes me think that the Operation power library is only designed for simple points.

Has anyone had to animate objects with double point? so that he can help me?

Thank you!!!!

Best regards,

Sebastian Contreras

  • Thumbnail of EcoStruxure™ Power Operation
    Schneider Electric
    EcoStruxure™ Power Operation
View products (1)
Labels
  • Labels:
  • Legacy Gateways & Energy Servers
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Romain_Polette
Kirk Romain_Polette Kirk
Kirk

Posted: ‎2023-01-17 05:03 AM . Last Modified: ‎2025-10-08 05:55 AM

0 Likes
0
1731
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
‎2023-01-17 05:03 AM

Hello, 

 

 

Please ask your question on the following section:

https://community.se.com/t5/EcoStruxure-Power-Operation/bd-p/power-scada-operation

 

Thanks.

 

Romain POLETTE
Solution Architect - France Operations

See Answer In Context

Reply
Replies 4
Romain_Polette
Kirk Romain_Polette Kirk
Kirk

Posted: ‎2023-01-17 05:03 AM . Last Modified: ‎2025-10-08 05:55 AM

0 Likes
0
1732
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
‎2023-01-17 05:03 AM

Hello, 

 

 

Please ask your question on the following section:

https://community.se.com/t5/EcoStruxure-Power-Operation/bd-p/power-scada-operation

 

Thanks.

 

Romain POLETTE
Solution Architect - France Operations
Reply
jaysonlkh
Ensign jaysonlkh Ensign
Ensign

Posted: ‎2023-03-06 05:38 AM

0 Likes
0
1596
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
‎2023-03-06 05:38 AM

Hi,

 

I will suggest you create 4 different dynamic objects and using hide condition to perform this. There is no multiple dynamics in our library.

 

Thank you.

 

Regards,

Hafidz Lee

Reply
Dhananjay2
Ensign Dhananjay2 Ensign
Ensign

Posted: ‎2023-07-10 09:34 PM

0 Likes
0
1399
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
‎2023-07-10 09:34 PM

Try to use array expression 

 Symbol Set Properties - Appearance General (Array)

Symbol Set Properties - Appearance General (Array)

Symbol Sets have the following general appearance (Array) properties:

PropertyDescription

Array expression

Enter the expression which is to return one or more integers. For each returned integer, a different symbol will be displayed.

If the return value is:

  • Less than 0 (zero), it will be set to 0 (zero), and a runtime hardware alarm will be triggered.
  • Greater than 255, it will be set to 255, and a runtime hardware alarm will be triggered.
  • A real (non-integer) number, it will be rounded off to the nearest integer.

To insert a tag or a function, click the Wizard button to the right of this field. This button displays two options; Insert tag, and Insert Function.

Array symbol

The symbol that is to display for each integer returned by the Array expression entered above (symbol 0 will be used when the expression returns integer 0, symbol 1 will be used when integer 1 is returned etc.).

Click the Set button to select a symbol, or Clear to clear the current selection.

For example, to display different symbols illustrating the various states of a motor, you could fill out the Array expression and Array symbol fields as follows:

 

 

In this example, MOTOR_STATUS is an analog variable tag representing the status of a motor. Each time the motor changes state, an integer is returned (0 = Running, 1 = Starting etc.), and the appropriate symbol displays.

Reply
Hryhorenko_ActiVolt
Crewman Hryhorenko_ActiVolt
Crewman

Posted: ‎2025-10-07 06:32 AM

0 Likes
0
382
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
‎2025-10-07 06:32 AM

In most of components is function "isValidValue" that blocks any value exept 0 and 1, the simplest way is to rewrite component to accomodate your need for DPI instead of SPI. It's not that hard to be honest, but be aware that you might need to set custom postitions if component doesn't have intermediate and error conditions built in
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.