Animation of double signal switches in IEC61850 Power Operation
Hello everyone!
Please help me on the following topic!
We need to animate an HMI, which refers to a substation, here we have to animate the switches with double points, these points are given to me by the CID file, specifically from the SCSWI1.Pos.StVal node (IEC61850 node), this node has 4 states : 0, 1, 2 and 3.
But when it comes to animating the object, it only takes states 0 and 1, therefore, it makes me think that the Operation power library is only designed for simple points.
Has anyone had to animate objects with double point? so that he can help me?
Thank you!!!!
Best regards,
Sebastian Contreras
- Labels:
-
Legacy Gateways & Energy Servers
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
Hello,
Please ask your question on the following section:
Thanks.
Solution Architect - France Operations
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
Hi,
I will suggest you create 4 different dynamic objects and using hide condition to perform this. There is no multiple dynamics in our library.
Thank you.
Regards,
Hafidz Lee
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
Try to use array expression
Symbol Set Properties - Appearance General (Array)
Symbol Sets have the following general appearance (Array) properties:
PropertyDescriptionArray expression | Enter the expression which is to return one or more integers. For each returned integer, a different symbol will be displayed. If the return value is:
To insert a tag or a function, click the Wizard button to the right of this field. This button displays two options; Insert tag, and Insert Function. |
Array symbol | The symbol that is to display for each integer returned by the Array expression entered above (symbol 0 will be used when the expression returns integer 0, symbol 1 will be used when integer 1 is returned etc.). Click the Set button to select a symbol, or Clear to clear the current selection. For example, to display different symbols illustrating the various states of a motor, you could fill out the Array expression and Array symbol fields as follows:
In this example, MOTOR_STATUS is an analog variable tag representing the status of a motor. Each time the motor changes state, an integer is returned (0 = Running, 1 = Starting etc.), and the appropriate symbol displays. |