Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Hello everyone!
Please help me on the following topic!
We need to animate an HMI, which refers to a substation, here we have to animate the switches with double points, these points are given to me by the CID file, specifically from the SCSWI1.Pos.StVal node (IEC61850 node), this node has 4 states : 0, 1, 2 and 3.
But when it comes to animating the object, it only takes states 0 and 1, therefore, it makes me think that the Operation power library is only designed for simple points.
Has anyone had to animate objects with double point? so that he can help me?
Thank you!!!!
Best regards,
Sebastian Contreras
Link copied. Please paste this link to share this article on your social media post.
Hello,
Please ask your question on the following section:
Thanks.
Link copied. Please paste this link to share this article on your social media post.
Hi,
I will suggest you create 4 different dynamic objects and using hide condition to perform this. There is no multiple dynamics in our library.
Thank you.
Regards,
Hafidz Lee
Link copied. Please paste this link to share this article on your social media post.
Try to use array expression
Symbol Sets have the following general appearance (Array) properties:
PropertyDescriptionArray expression | Enter the expression which is to return one or more integers. For each returned integer, a different symbol will be displayed. If the return value is:
To insert a tag or a function, click the Wizard button to the right of this field. This button displays two options; Insert tag, and Insert Function. |
Array symbol | The symbol that is to display for each integer returned by the Array expression entered above (symbol 0 will be used when the expression returns integer 0, symbol 1 will be used when integer 1 is returned etc.). Click the Set button to select a symbol, or Clear to clear the current selection. For example, to display different symbols illustrating the various states of a motor, you could fill out the Array expression and Array symbol fields as follows:
In this example, MOTOR_STATUS is an analog variable tag representing the status of a motor. Each time the motor changes state, an integer is returned (0 = Running, 1 = Starting etc.), and the appropriate symbol displays. |
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.