Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
This forum is for engineers working EcoStruxure Building Operation, wanting to leverage the SEAL application to improve the efficiency in the engineering process.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-19 01:44 AM
Hi,
I am able to get the list of properties for the objects, but I am not able to retrieve their values. Is there a way to do this? I can even update or create the objects, but reading their values is also important and should be possible.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-19 07:59 AM . Last Modified: 2025-08-19 08:06 AM
Try the attached Demo Script , it might help you.
If you have the below objects on your server you should be able to read the values of different properties with the script, ensure you select the correct data type for the specific property you want to read.
If you want to read the 'Display on alarm' property for the 'Change of State Alarm' object in the above example you configure the demo script as below ( The attachment is a hidden child object to the alarm named 'Attachment' , and the property to read is 'Popup' , data type = Boolean)
I hope this helps you
/Stefan
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-19 06:04 AM
Hi @mtalhagaoglu
Is this regarding SEAL script ?
If so, yes you should be able to retrieve the value also.
Is it values on AS or MP/RP devices you got problem with ?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-19 06:53 AM
Hi Stefan,
Yes, this is related to the script part of SEAL.
The method I am using is sdkClient.IAdvanced.GetPropertyValueVariableReference, and the response I get is as follows:
{"failed":false,"message":"","nativeValue":0,"returnValue":{"value":null,"transferRateSeconds":0,"retransmitMinutes":0,"deltaFilter":0,"isNull":true,"isLocked":false,"isRelative":false,"isServerAbsolute":false,"isSystemAbsolute":false,"_dotNetType":"VariablesPropertyReference"},"status":"Ok","trace":""}
I can get string values of the point, such as name and description, but the actual value is always null. It allows me to update it, but reading seems to be the issue.
Additionally, I wasn’t able to get the "Display on alarm" status of an alarm attachment.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-19 07:59 AM . Last Modified: 2025-08-19 08:06 AM
Try the attached Demo Script , it might help you.
If you have the below objects on your server you should be able to read the values of different properties with the script, ensure you select the correct data type for the specific property you want to read.
If you want to read the 'Display on alarm' property for the 'Change of State Alarm' object in the above example you configure the demo script as below ( The attachment is a hidden child object to the alarm named 'Attachment' , and the property to read is 'Popup' , data type = Boolean)
I hope this helps you
/Stefan
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-22 07:05 AM . Last Modified: 2025-08-22 07:11 AM
Hi Stefan,
Thank you for the script and your guidance.
The script helped me retrieve the value of the "Analog Value" point, but I couldn’t access the Popup property of the alarm attachment.
"Display on alarm" is bound to this property path: /Server 1/Change of State Alarm/Test Attachment 1/Popup
"Test Attachment 1" is the name of the attachment, but unfortunately, we can’t see this value in the attachment list of the alarm.
All of their names look like "Analog Value," but the real name can be found the xml file or the alarm's properties popup.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-22 08:38 AM
Hi again,
I tested your setup and have no issue reading binary state of the popup property using the demo script :
Script config to Read the state of 'Test Attachment 2' :
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-08-25 12:12 AM
Hi Stefan,
I can read the popup status using the property path "/Server 1/Change of State Alarm/Test Attachment 1/Popup". I just wanted to share this in case other users get stuck in the same situation with the attachment name.
Thank you again for your help.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.