Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

An example for 'determining the smallest allowable cross-sectional area of circuit conductors.'

Power Distribution and Digital Support

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.
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
  • Power Distribution IEC
  • Power Distribution and Digital Support
  • An example for 'determining the smallest allowable cross-sectional area of circuit conductors.'
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Genghiz
Captain Genghiz Captain
93
Gregoire_Brun
Commander Gregoire_Brun Commander
80
J_Travostino
Sisko J_Travostino Sisko
70
View All

Recommended Forums

  • Comunidade de Soluções Elétricas

  • Expert on Demand for Standards & Regulations

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Power Distribution and Digital Support
Start a Topic
Solved
Genghiz
Captain Genghiz Captain
Captain

Posted: ‎2020-11-09 11:59 PM . Last Modified: ‎2024-11-22 04:25 AM

1 Like
1
3482
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
Posted: ‎2020-11-09 11:59 PM . Last Modified: ‎2024-11-22 04:25 AM

An example for 'determining the smallest allowable cross-sectional area of circuit conductors.'

From the available inputs;

let us see how to determine the 'smallest allowable cross sectional area' of the circuit conductors.

 

Available inputs;

 

Load Current

200 A

THDi

48 %

Conductor Insulation*

XLPE

Conductor Type

Multi-Core Cable

Conductor Material*

Copper

Installation

Directly in Ground

Soil Resistivity*

2 Km/w

Soil Temperature*

40*C

 

*Some of the inputs are assumed to provide in this example; and they were neither received from the user, nor from the environment.

 

 

Procedure:

 

  • Determinant conductor : Neutral

          As the THDi is > 33 % (that is THDI = 48 %). So, the Size-determining" live conductor is Neutral

 

  • Neutral Current               :  3 × 0.48 × 200 = 288 A

 

  • Correction factor K3       : The factor based on the overload protection device.

           This circuit is assumed to be protected by the circuit-breaker.

           So that the K3 =1.0

 

  • F1 Temperature              : Table B.52.15

          For 40°C and with the insulation XLPE. F1 = 0.85

 

  • Installation method       : 72                                                                                                           (Sheathed single-core or multi-core cables direct in the ground - without added mechanical protection) Reference method          : D2

                                          

  • F2 Group                          : Table B.52.18

          There is no additional touching circuits i.e. total no. of circuits is 1

          F2group = 1.00

 

  • Correction factor F3       : Table (E.52.1)

          THDI >45 % = THDI = 48 %  à f3NeutralTHDI = 1.00

 

  • F3RSoil                              : Table B.52.16

           Installation method = in Ground -> Rth = 2.0 K.m/w

           f3RthSoil = 1.12  

    

  • K user = 1.0

 

Correction factor f

f = 0.85 × 1.00 × 1.00 × 1.05 × 1.00 = 0.952

The overall correction factor is determined by multiplying all 'the available correction factors."

 

 

Theoretical Iz’                 = (K3 x IB) / (F x N live) = (1.0 x 288) / (0.952 x1) = 302.52 A = 303 A

The conductor selection is done from the given Table B.52.5 Column 8 

185 mm2 will be able to carry 324 Amps

240 mm2 will be able to carry 375 Amps

Considering the +5% of tolerance, It would be recommended to consider the size as 185 mm²

 

K3(Correction Factor based on Protection Device)

1

F1(Correction Factor based on Temperature)

0.85

F2(Correction Factor based on Group of conductors)

1

F3(Correction Factor based on THDi)

1

F3(Correction Factor based on Soil Resistivity)

1.05

K user(Correction Factor defined by the user)

1

 

 

Iz’(A) Theoretical

303 A

Iz (A) considered from the table

324 A

Theoretical cross sectional area  Ph (mm²)

1 x 185   mm²

Theoretical cross sectional area Neutral (mm²)

1 x 185   mm²

Theoretical cross sectional area PE (mm²)

1 x 95   mm²

 

 

Labels
  • Labels:
  • Power Distribution Software
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
dkpElect
Crewman dkpElect
Crewman

Posted: ‎2021-06-26 05:32 AM

1 Like
0
3225
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
Posted: ‎2021-06-26 05:32 AM

That's really informative answer. 

Thanks.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
dkpElect
Crewman dkpElect
Crewman

Posted: ‎2021-06-26 05:32 AM

1 Like
0
3226
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
Posted: ‎2021-06-26 05:32 AM

That's really informative answer. 

Thanks.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.