Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the Schneider Electric Community! We have moved to a new address: community.se.com — bookmark it today and contact SchneiderCommunity.Support@se.com if you have any questions!
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82740members
350508posts

SNMP trap

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Mohamed_Fahmy
Ensign Ensign
Ensign
0 Likes
3
1310

SNMP trap

Hello,

 

I need to send SNMP trap from DCE server and netbotz 450 to a third party SNMP trap receiver (NNMi) from HP. So is it necessary to upload the MIB file of the netbotz on the trap receiver to receive traps from DCE and netbotz?

 

thanks,

Mohamed Magdy

 

3 Replies 3
TechieBala
Ensign Ensign
Ensign

Re: SNMP trap

Dear @Mohamed_Fahmy ,

 

Yes, NMS systems normally require the MIB files to be uploaded. Please refer the below k-base document which addresses your query.

https://www.se.com/in/en/faqs/FA231439/

 

Struxureware DCE Powernet MIB can be downloaded in the below link:
https://www.apc.com/shop/in/en/products/PowerNet-MIB-v4-3-2/P-SFPMIB432

 

The SNMP MIB for NetBotz Appliances can be downloaded from the NetBotz Appliance itself by accessing the following URL:
V3
http://ip_address_of_appliance/netbotzv3.mib

 

The latest MIB should also be available on the APC software downloads page at:
https://www.apc.com/shop/us/en/products/NetBotz-MIB-v3-2-0/P-SFNBMIB320

 

You can configure your NMS or Trap Receiver on DCE Dekstop client.

NMS1.pngNMS2.pngNMS3.png

 

I hope this helps. 

 

Mohamed_Fahmy
Ensign Ensign
Ensign
0 Likes
1
1242

Re: SNMP trap

we made the configuration in the DCE as you mentioned, downloaded the MIB file direct from the netbotz and uploaded it in the NMS but we can not receive the traps on NMS. we test flow on the network we found that the netbotz send the below trap but we can not see this trap on NMS:

10.1.91.13.1024 > nnmipr1.snmp: [udp sum ok]  { SNMPv1 C= ????{ Trap(424)  E:5528.100.10.2.1 10.1.91.13 enterpriseSpecific s=2 7839703 E:5528.100.11.1="nbErrorCond_4C4344C1" E:5528.100.11.2="nbErrorType_toohigh" E:5528.100.11.3="Value Too High" E:5528.100.11.4="nbAlinkEnc_0_2_TEMP" E:5528.100.11.5="OFY.ICT1.F06/SrT09" E:5528.100.11.6="nbAlinkEnc_0" E:5528.100.11.7="Sensor Pod" E:5528.100.11.8="" E:5528.100.11.9="" E:5528.100.11.10=1582636987 E:5528.100.11.11=1582636987 E:5528.100.11.12=0 E:5528.100.11.13=3 E:5528.100.11.14="22.4 __C" E:5528.100.11.15=22 E:5528.100.11.16=399999 } }

we notice that the OIDs is not the same as in MIB (it is not complete Ex: E:5528.100.11.2 should be 1.3.6.1.4.1.5528.100.11.2 )

 

please advise where is the problem?

TechieBala
Ensign Ensign
Ensign
0 Likes
0
1238

Re: SNMP trap

I suggest you to use the SNMP Trap test by using DCE "Network Management Systems Integration" feature and see if it has different results. To use DCE "Network Management Systems Integration" feature, then please use Powernet MIB instead of Netbotz MIB.
I am not familiar in NNMi NMS. The DCE SNMP Trap feature works as the way it is described in the k-base document:FA231439. Capture.JPG
I also let other folks in this community to share their views on your query.