Posted: 2020-07-03 03:40 PM . Last Modified: 2024-04-08 12:53 AM
PUE graph does not match the figure
Dear expert,
We have configured PUE/EE and found that when the number is larger than 5, the graph of PUE does not match the figure. For example, in the pic I attached, the PUE number is 16, and in graph, it is in the place which is less than 1. And for PUE number is 44, in graph, it is in the place between 4 & 5.
What is the reason for that?
Thanks,
Ziqiang
(CID:117999538)
- Labels:
-
Data Center Operation
Link copied. Please paste this link to share this article on your social media post.
Accepted Solutions
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
Posted: 2020-07-03 03:40 PM . Last Modified: 2024-04-08 12:53 AM
Hi Ziqiang,
Out of curiosity, is it just a test or do you have data center(s) with PUE over 5 ?
As far as I know it was basically (by design) assumed that the usual PUE for a data center could be something between 1 and 5, and therefore the graphical presentation can only show numbers between 1-5.
The text format of the PUE can display the calculated numbers.
Kind regards
(CID:117999890)
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
Posted: 2020-07-03 03:40 PM . Last Modified: 2024-04-08 12:53 AM
Hi ziqiang wu,
thanks for posting. Lets see who can be of assistance here. @community any ideas?
Kind regards Ditte
(CID:117999654)
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
Posted: 2020-07-03 03:40 PM . Last Modified: 2024-04-08 12:53 AM
Hi Ziqiang,
Out of curiosity, is it just a test or do you have data center(s) with PUE over 5 ?
As far as I know it was basically (by design) assumed that the usual PUE for a data center could be something between 1 and 5, and therefore the graphical presentation can only show numbers between 1-5.
The text format of the PUE can display the calculated numbers.
Kind regards
(CID:117999890)
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
Posted: 2020-07-03 03:40 PM . Last Modified: 2024-04-08 12:53 AM
Hi Jef,
It's a pre-configure in customer's site, because some of the devices have not been online so the PUE is not quite reasonable. I'm just wondering if it is bug, if so, should we fix this?
Thanks,
Ziqiang
(CID:117999897)
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
Posted: 2020-07-03 03:40 PM . Last Modified: 2024-04-08 12:53 AM
Hi Ziqiang,
Many thanks for the update - no, that's not a bug - it is working as designed, thanks.
Kind regards
(CID:117999900)
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
Posted: 2020-07-03 03:40 PM . Last Modified: 2024-04-08 12:53 AM
Hi Jef,
But if you check the dashboard, the location of the indicator does not point to the place it should be located (larger than 5). Why is that?
Thanks,
Ziqiang
(CID:117999921)
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
Posted: 2020-07-03 03:40 PM . Last Modified: 2024-04-08 12:53 AM
Hi Ziqiang,
As you might have noticed the pointer might have circled several times and then ended up in a 'random' place - as mentioned the indicator can show correctly between 1 and 5.
Kind regards
(CID:117999975)
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
Posted: 2020-07-03 03:40 PM . Last Modified: 2024-04-08 12:53 AM
Thank you Jef.
(CID:117999982)
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
Posted: 2020-07-03 03:41 PM . Last Modified: 2024-04-08 12:53 AM
You are most welcome, Ziqiang
Kind regards
(CID:117999990)
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
Posted: 2020-07-03 03:41 PM . Last Modified: 2023-10-22 03:31 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.