EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-04 02:57 PM . Last Modified: β2024-04-05 02:28 AM
Hello,
I'm trying to read values from a couple of SNMP power strips working in a Master-Slave basis. They use one simple IP address. How can I add them to different devices in DCE? Is it possible?
Thanks in advance
(CID:129404692)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-04 02:57 PM . Last Modified: β2024-04-05 02:28 AM
Hi Antonio,
If the devices share an IP, DCE will see them as a single device. There's nothing you can do to add a full device unless you were to add the second one with a different IP.
The only other thing you can do is to create a virtual sensor for values that you would like to see as separate entities. If you have a pdu that has outlet current or wattage associated to it, you can create a virtual sensor associated with that value or a sum of the values of numerous sensors.
Steve
(CID:129404704)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-04 02:57 PM . Last Modified: β2024-04-05 02:28 AM
Steve,
it is not acceptable to have hundreds of virtual sensors for this kind of power strips.
Are you planning to add this feature?
Antonio
(CID:129406978)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-04 02:57 PM . Last Modified: β2024-04-05 02:28 AM
Hi Antonio,
I am not aware of any current DCE initiative to be able to separate devices that are linked under a single IP. You can always request this as an enhancement though by using the resources / feature request menus above.
I do understand that it is quite time consuming and would potentially make a huge number of virtual sensors to be able to use that functionality but that's also why I noted first that you may want to add the devices individually if they need to be seen as separate devices in DCE.
Steve
(CID:129406981)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-04 02:57 PM . Last Modified: β2023-10-22 02:32 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.