Posted: 2020-07-03 01:31 PM . Last Modified: 2024-04-08 01:36 AM
Error DCO
Hi
I lost communication with the DCO server and it shows me the message failed
and in Webmin
Failed to write to /var/webmin/modules/webmin/oscache when closing : No space left on device
What should I do
Regards
Norberto Castillo
(CID:113641762)
- Labels:
-
Data Center Operation
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
Posted: 2020-07-03 01:31 PM . Last Modified: 2024-04-08 01:35 AM
Hi Norberto,
I would go for a fresh/clean installation of DCO and then restoring the latest successful backup file.
If not running the latest version already, then go for DCO 8.0.4 - specially if you should be running 8.0.0. There is a known issue with 8.0.0, that log files can grow in some setups and potentially can take up all disc space.
The scheduled daily backup files usually located on the local disc "/data/backup" folder, and can be accessed/downloaded either via server Webmin interface or by using tools such as WinSCP.
For the installation, at least 100 GB storage/disc space is the minimum recommendation.
Kind regards
(CID:113641967)
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
Posted: 2020-07-03 01:31 PM . Last Modified: 2024-04-08 01:36 AM
Hi
The message is
(CID:113641959)
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
Posted: 2020-07-03 01:31 PM . Last Modified: 2024-04-08 01:35 AM
Hi Norberto,
I would go for a fresh/clean installation of DCO and then restoring the latest successful backup file.
If not running the latest version already, then go for DCO 8.0.4 - specially if you should be running 8.0.0. There is a known issue with 8.0.0, that log files can grow in some setups and potentially can take up all disc space.
The scheduled daily backup files usually located on the local disc "/data/backup" folder, and can be accessed/downloaded either via server Webmin interface or by using tools such as WinSCP.
For the installation, at least 100 GB storage/disc space is the minimum recommendation.
Kind regards
(CID:113641967)
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
Posted: 2020-07-03 01:31 PM . Last Modified: 2024-04-08 01:35 AM
Dear Jef
Checking the PUE values only shows me the history until 02-Feb.
The DCO does not show the PUE values of the last 2 days (5 and 6Feb)
(CID:113642511)
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
Posted: 2020-07-03 01:31 PM . Last Modified: 2024-04-08 01:35 AM
Hi Norberto,
Sounds great that it's working now. But this is a new issue and could have been posted as a new community post/"question" 😀 I would be happy to look into this PUE issue. Would iit be possible to ask for the following data:
. latest backup file
. server logs (can be downloaded from webmin interface: StruxureWare DC Operation > Download Log Files > "Download log file")
I will send you an invite to my =S= box, so the files can be safely shared with me, thanks.
Kind regards
(CID:113642885)
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
Posted: 2020-07-03 01:32 PM . Last Modified: 2024-04-08 01:35 AM
Hi Jef
I delete and create the partition of hard disk then install the DCO ver 8.0
I can calculate the PUE in dashboard
Is it necessary to wait days to see the history of the PUE? (see image of DCE integration)
I don´t see any errors at the configuration of PUE
Please tell me your email and I will send you the information you request
Thanks you
(CID:113643299)
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
Posted: 2020-07-03 01:32 PM . Last Modified: 2024-04-08 01:35 AM
Hi Norberto,
Many thanks for the info & providing the data, I will study the files and will get back to you as soon as possible.
Kind regards
(CID:113643302)
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
Posted: 2020-07-03 01:32 PM . Last Modified: 2024-04-08 01:35 AM
Hi Norberto,
I have studied the kindly provided data, and it seems the latest calculated PUE's have been on 2017-03-02 02:30, and then the calculation have not been successful. That seems to be basically due to:
the failing script apparently associated to "UPS RAMAL"
error in scripts for "Consumo Ramal A + externo" and "UPS Ramal B + externos"
Furthermore, the 'Typical PU' and 'Usable fraction of nameplate w/o derating' seems to be mis-configured for the Switch gear in the EE energy system (they should not be set to zero), you might want to change the Typical PU to 2 and the Usable fraction of nameplate w/o derating to 1.
PS: currently the "Evaluate Energy System" may display "No data" (as you have illustrated) if the system is not properly setup.
Kind regards
(CID:113644278)
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
Posted: 2020-07-03 01:32 PM . Last Modified: 2024-04-08 01:35 AM
Hi Jef
Thank you very much for your help
(CID:114231263)
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
Posted: 2020-07-03 01:32 PM . Last Modified: 2024-04-08 01:35 AM
Hi Norberto,
Excellent, many thanks for sharing, appreciated.
Kind regards
(CID:114231265)
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
Posted: 2020-07-03 01:32 PM . Last Modified: 2023-10-22 02:02 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.