Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84577members
353848posts

DCO generating multiple authentications requests on active directory once logged on

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

RCastillo
Crewman
Crewman
0 Likes
1
331

DCO generating multiple authentications requests on active directory once logged on

 

Once logged on, active directory is getting multiple authentication requests from DCO.

 

Do you guys have any idea what would cause it? 

 

 

 

 

Attachments
Tags (1)
1 Reply 1
gsterling
Commander Commander
Commander
0 Likes
0
277

Re: DCO generating multiple authentications requests on active directory once logged on

Hello Jose

 

Without reviewing log information from your server to check into your case specifically, I can tell you DCO/ITA does limit its use of the login credentials to just the initial authentication to the DCO/ITA server.

 

This is at least partly because many of the api calls made by the desktop and web clients must successfully authenticate before they can be completed. This behavior also adds an additional level of security to DCO/ITA which security auditors may require as it means if a DCO/ITA users access were removed while they were using the product, their access is nearly immediately revoked. The customer does not need to wait for the user to logoff.

 

Regards

 

Greg Sterling 

Tags (1)