Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 08:59 PM . Last Modified: 2024-04-03 01:01 AM
Hi Team!
Could you point me if there some significant difference between power distribution objects in DCO?
Basically we have Generic PDU, Generic Power Panel, Generic Remote Distribution panel with 1-phase and 3-phase options.
is there some difference between them when DCO proceed power dependency?
May be each of them have unique features?
Or this different types was made only for user convenience and are the same from DCO point of view?
(CID:147198266)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 08:59 PM . Last Modified: 2024-04-03 01:01 AM
Hello Valentin.
Its my understanding most of the above power devices you asked about are provided for the customers convenience so that item names/types align with the equipment in their actual data center.
They are in general similar in capabilities. They all have breaker panels, support a single input feed and can distribute to multiple devices. One difference to note is that PDU's and Power Panels also give you the ability to specify an output voltage so pdu's and power panels can be configured as a step-up or step-down device from a voltage standpoint.
Remote distribution panel voltages are set based on the device which feeds them. Here's a sample power properties view for a three phase remote distribution panel.

where as a pdu/power panel allows the customer to define its input feed as well as its output power. Here's a sample power properties view for a pdu.

Also, given you are allowed to define the input voltage and breaker settings on devices like PDU's this means these devices can be the first device on a power path. A UPS does not have to be the first device when those settings are provided.
Regards
Greg Sterling
(CID:147201746)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 08:59 PM . Last Modified: 2024-04-03 01:01 AM
Thank you Greg!
Very clear 🙂
(CID:147201750)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 08:59 PM . Last Modified: 2023-10-22 03:36 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.