Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-06 12:13 AM . Last Modified: 2024-04-02 11:39 PM
Hi all, I just wanted to share some important info on the 4.7 release of BotzWare. This will come into play on any new NetBotz device or any device running 4.7 that is reset to defaults:
Product Line:
NetBotz
Environment:
NetBotz version 3, NBWL0355, NBRK0450, NBWL0455, NBRK550, NBRK570
With the introduction of new California State legislation (SB-327), which comes into effect from January 1st, 2020, any manufacturer of a device that connects “directly or indirectly” to the internet must equip it with “reasonable” security features, designed to prevent unauthorized access, modification, or information dis-closure. APC by Schneider Electric (APC) network-enabled devices firmware is updating in compliance with this legislation.
The following are the overview of changes which will come into effect with this new Botzware 4.7.0 version. Please communicate to your FSR team members who deals Netbotz configuration in the field.
1. WEB access will be OFF by default -> the customer will need to login via the USB console using root/apc and setup a new password which will then enable HTTPS access only
>They will then be able to login via HTTPS using the apc username and the new password they just set
2. The serial config utility will no longer work – will need to use a terminal program instead
Warning: system login through this interface without direction
from NetBotz Support will void your warranty.
netbotzDD3A7B login: root
Password:
Linux (none) 2.6.12 #307 Tue Jul 9 12:11:47 EDT 2019 ppc unknown
Welcome to NetBotz BotzWare V4.7.0
***************************************************************************
* To increase security, initial access to new NetBotz appliances has been *
* limited to this command console. *
* Once the Root password is set here, you can access the WEB UI and *
* use Advanced View and Data Center Expert to configure the appliance. *
* Only HTTPS (TCP port 443) will be enabled at that time *
***************************************************************************
New password:
Retype new password:
Thanks,
Steve
(CID:152570349)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-06 12:13 AM . Last Modified: 2024-04-02 11:39 PM
Just an FYI, this only effects a new install or an appliance that's been reset to defaults. Devices upgraded from earlier versions will not have these changes to the protocols or require password changes.
(CID:152570552)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-06 12:13 AM . Last Modified: 2023-10-22 03:27 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.