Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 11:43 PM . Last Modified: 2024-04-03 12:03 AM
Hi all,
in phased projects, one site per phase, once one site DCO is delivered to the customer, the start working with it, adding, removing items, etc... But we need to build other sites separately in other DCO instance and once finished, we should be able to add/merge the new site with the first one in production environment. I tried with Migration from Struxuware Operation option, but it seems not to work.
How does it works? Is there other way to do that?
Thanks
(CID:152077773)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 11:43 PM . Last Modified: 2024-04-03 12:03 AM
Hi Antonio,
I would also have suggested using the migration feature, however please note that:
Example A)
1) clean install of DCO on server1 (and then do your work)
2) clean install of DCO on server2 (and then do your work)
These two installations (and their setups) are unique, so we can successfully migrate data from one server onto another. Migration can be done only once!
Example B)
1) clean install of DCO on server1
2) clean install of DCO on server2, and then restore a backup from server1, modify the setup, add rooms, etc.
These two installations are not unique even though they may contain completely different rooms/locations. By restoring a backup file, server2 may get the similar origin as server1.
In this case migration will fail!
Kind regards
(CID:152077784)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-05 11:43 PM . Last Modified: 2023-10-22 02:32 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.