Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 01:32 AM . Last Modified: 2024-04-09 12:34 AM
Hello community
I have a problem trying to send e-mails with DCO, for the first time. In fact, when I'm doing a test on "e-mails settings", it fails displaying the following message:
"Test e-mail could not be sent. This could be caused by relay restrictions. See the server log for more information"
Also, when trying to send an e-mail by command:
root@host:~# mail -s "Hello world" e-mail (CTRL-D)
/usr/lib/sendmail: No such file or directory
root@host:~# "/root/dead.letter" 9/216
. . . message not sent.
My question is: do we need to setup sendmail/Postfix, in order to have DCO e-mail working?
What are we missing?
I do also did a test on Webmin using the "Send Mail" option and it indicates that there's no mail program installed on the system.
Can we install sendmail/postfix webmin module?
Thanks for your help and advise!
(CID:105469965)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 01:32 AM . Last Modified: 2024-04-09 12:34 AM
Hello all
I want to confirm that our problem was related to a firewall restriction and now it's working.
To summarize, as Greg pointed, the email client is configured using the DCO> e-mail settings, from the DCO GUI Client. And as Bala mentioned: "Information required is SMTP server IP address, port # and authentication(if applicable)."
In addition, I included a verification of the network connectivity from the DCO server to the smtp server (A PING, also a verification of the port, if it's reachable: usually a telnet smtp_server_ip smtp_server_port would work or any other tool to confirm connectivity, ex: openssl)
Additional step, if it continues failing, it's to " white list the DCO IP address or provide permission for DCO IP address to send an email" as Bala recommended.
Thanks everybody for your help!
(CID:105470342)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 01:32 AM . Last Modified: 2024-04-09 12:34 AM
Angelica.
Are you trying to configure emails from DCO? This is normally completed using the DCO client GUI. Under the system settings menu is the email settings option from which you can configure your SMTP settings for DCO emails.
Are you attempting to configure linux email from the DCO server for another reason?
Regards
Greg Sterling
(CID:105469991)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 01:32 AM . Last Modified: 2024-04-09 12:34 AM
Hi Greg, thanks for your answer. I've been trying to use the DCO client GUI and it doesn't work. For this reason I wanted to confirm with you and the community if my installation is uncompleted and needing additional setup as I didn't see any email client installed. But Now I'm clear that the only thing we need is the DCO client GUI. Thanks for the clarification. Now I'm trying to have the smtp test setup using the GUI but still no luck.
(CID:105470211)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 01:32 AM . Last Modified: 2024-04-09 12:34 AM
Dear Angelica,
I have faced this issue in one of the Customer DCO implementations recently. I have asked the Customer to whitelist the DCO IP address in their Mail Exchange server which resolved the issue.
As the error message points that "This could be caused by relay restrictions.", you will need to ask your Mail Exchange Server team to white list the DCO IP address or provide permission for DCO IP address to send an email.
Please make sure that SMTP server IP address, port # and authentication(if applicable) are entered correctly using the DCO client GUI.
It should resolve this issue.
Regards,
Bala
(CID:105470066)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 01:32 AM . Last Modified: 2024-04-09 12:34 AM
Hi Bala Thanks for your answer and it gave me a light. At this moment we're using a basic test with gmail/yahoo accounts. I've managed to verify if the server has connectivity to the smtp server, and it doesn't. So my guess is that the firewall is restricting this connection. I'll confirm if this is the solution or if the problem persists. Thanks!
(CID:105470213)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 01:32 AM . Last Modified: 2024-04-09 12:34 AM
Hello all
I want to confirm that our problem was related to a firewall restriction and now it's working.
To summarize, as Greg pointed, the email client is configured using the DCO> e-mail settings, from the DCO GUI Client. And as Bala mentioned: "Information required is SMTP server IP address, port # and authentication(if applicable)."
In addition, I included a verification of the network connectivity from the DCO server to the smtp server (A PING, also a verification of the port, if it's reachable: usually a telnet smtp_server_ip smtp_server_port would work or any other tool to confirm connectivity, ex: openssl)
Additional step, if it continues failing, it's to " white list the DCO IP address or provide permission for DCO IP address to send an email" as Bala recommended.
Thanks everybody for your help!
(CID:105470342)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 01:33 AM . Last Modified: 2023-10-31 10:47 PM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.