Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 09:02 PM . Last Modified: 2024-04-04 03:58 AM
I have a query related to the DCE system for one of our customer
Let me give you the detailed structure of our system
We have 17 sites of BMS which we have integrated with our system DCE
We are using 1 server for DCE and almost more than 8000 sensors are integrated for 17 BMS sites (virtual sensors not the apc)
We have created 17 separate DCE virtual machines in 1 server (each DCE has its own IP)
But our plan is to merge all DCE VM into 1 VM, which means merging all sensors of each site into 1 IP (into 1 DCE)
We have placed Protocol converters which are directly communicating with the BMS sites through Bacnet Protocol (We normally enter the IP address of the BMS system and Bacnet instance number in the PC converters) than the OID'S are generated and same OID'S we manually add into the DCE and via ETL integration we add it up on DCO
This is how the system is working ?
So instead of 17 DCE we need only 1 that is the idea
But my concern is that the database how it will be merged into one for 17 sites
We have manually created the virtual sensors each DCE has more than 300 sensors
Is it possible to merge all into 1 like copying or any solution?
Because if we will create 1 DCE how we are going to copy the data of the other 16 sites
We cannot manually enter again and create virtual sensors it will be a long process again then ?
Kindly suggest if its possible then how ?
If not then we need the detailed explanation, why its not possible and what are the risks ?
Regards
(CID:132670779)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 09:03 PM . Last Modified: 2024-04-04 03:58 AM
Hi Waseem
AFAIK no way to merge DBs and not sure about exporting virtual sensors. do that get created along with devices when exporting discovery entries? anyone?
in addition, depending on your polling frequency, you may find poor perf on a single combined system. make sure there is plenty of dedicated CPU & RAM and also important is IO performance check for this in iops (disk IOs per sec)
in the past I have recommended retaining old DCEs for historical data with polling stopped and polled on new DCE. u may consider overlapping polling to get some data into new DCE, eg one month
hope this helps
cheers
Ed
(CID:132670832)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 09:03 PM . Last Modified: 2024-04-04 03:58 AM
Hi Waseem
AFAIK no way to merge DBs and not sure about exporting virtual sensors. do that get created along with devices when exporting discovery entries? anyone?
in addition, depending on your polling frequency, you may find poor perf on a single combined system. make sure there is plenty of dedicated CPU & RAM and also important is IO performance check for this in iops (disk IOs per sec)
in the past I have recommended retaining old DCEs for historical data with polling stopped and polled on new DCE. u may consider overlapping polling to get some data into new DCE, eg one month
hope this helps
cheers
Ed
(CID:132670832)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 09:03 PM . Last Modified: 2024-04-04 03:58 AM
Hi Waseem,
As Ed mentioned, there is no database merge option. A backup/restore will only restore that 1 server's info and if you try to restore a second server's backup, it will overwrite the first.
You can export the discoveries of each of the servers and create a file including all of the discoveries to import and re-run on the new server.
As for the virtual sensors, they can not be exported and imported individually. The new DCE would have no way of knowing what to use for sensors to add or average. When creating a virtual sensor, DCE does not look at each sensor OID and IP. It looks at the unique identifiers of the device and it's sensors. This unique identifier is specific to this instance of DCE and to the specific discovery. If you were to delete and rediscover a device, the unique identifiers would be different even on the same server so you can see how a new server would not be able to map these sensors...sorry. To get these sensors on a new server, you will have to manually recreate them.
Steve
(CID:132670860)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 09:03 PM . Last Modified: 2024-04-04 03:58 AM
Hi Ed
Thanks for your reply
I have attached the screen shot of one of our dce system you can see 550 devices (sensors) and there are 2 SNMP devices those are actually the Protocol Converters through which we are getting the readings by adding supplemental OID'S.
So similarly we have 17 DCE'S the idea is to make them in 1 IP (1 DCE) only combining almost 8000 sensors
But we don't want to add it manually again because it will be a long process again ?
Merging all the DCE'S is that possible ?
db of DCE is SQL or not ?
Regards
(CID:132670876)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 09:03 PM . Last Modified: 2024-04-04 03:58 AM
Waseem,
As both Ed and I have stated, there is no way to merge the databases.
First, you do not have access to the database (psql). Secondly, the database only holds pointers to files and data that reside on the system as a computer directory structure so pulling database information would be of no use in the creation of a new server.
Steve
(CID:132670882)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 09:03 PM . Last Modified: 2024-04-04 03:58 AM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-04 09:03 PM . Last Modified: 2023-10-22 01:20 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.