Analogue and Digital Sensors with Serial RS-232 and EIA-485 Outputs

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • Analogue and Digital Sensors with Serial RS-232 and EIA-485 Outputs
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Admiral Cory_McDonald Admiral
129
Jef
Admiral Jef Admiral
111
gsterling
Captain gsterling Captain
72
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
Solved Go to Solution
Back to EcoStruxure IT Forum
Start a Topic
Solved
DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 01:48 AM . Last Modified: ‎2024-04-09 12:28 AM

0 Likes
4
1119
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
Posted: ‎2020-07-03 01:48 AM . Last Modified: ‎2024-04-09 12:28 AM

Analogue and Digital Sensors with Serial RS-232 and EIA-485 Outputs

Dear Team,

Kindly advise on how to connect the subject sensors to NetBotz appliance?

Regards,

Felix

(CID:105470476)

Labels
  • Labels:
  • NetBotz
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2024-04-09 12:28 AM

0 Likes
2
1119
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
Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2024-04-09 12:28 AM

Hi Felix,

 

NetBotz supports it's own sensors with either the version 2 DIN type connectors or the version 3 RJ45 type connectors. For 3rd party sensors, we support connecting sensors using dry contacts, 0-5 volt connections, or 4-20 Ma connections. These are usually 2 wire connections with a potential connection for power if applied by the NetBotz device. 

 

There are some devices such as the SeaLevel relay output type devices that are supported by the NetBotz devices and they connect via USB. We also support modbus output (not input) over IP and RS485 using an FTDI USB to RS485 cable as noted in the manual.

 

We do not directly support any RS232 or EIA-485 connection inputs. NetBotz devices are not capable at this time of monitoring devices using the modbus protocol. 

 

Thanks,

Steve

 

 

(CID:105470621)

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 4
DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2024-04-09 12:28 AM

0 Likes
2
1120
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
Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2024-04-09 12:28 AM

Hi Felix,

 

NetBotz supports it's own sensors with either the version 2 DIN type connectors or the version 3 RJ45 type connectors. For 3rd party sensors, we support connecting sensors using dry contacts, 0-5 volt connections, or 4-20 Ma connections. These are usually 2 wire connections with a potential connection for power if applied by the NetBotz device. 

 

There are some devices such as the SeaLevel relay output type devices that are supported by the NetBotz devices and they connect via USB. We also support modbus output (not input) over IP and RS485 using an FTDI USB to RS485 cable as noted in the manual.

 

We do not directly support any RS232 or EIA-485 connection inputs. NetBotz devices are not capable at this time of monitoring devices using the modbus protocol. 

 

Thanks,

Steve

 

 

(CID:105470621)

Reply

Link copied. Please paste this link to share this article on your social media post.

DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2024-04-09 12:28 AM

In response to DCIM_Support
0 Likes
0
1119
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
Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2024-04-09 12:28 AM

Hi Steven, Thank you for your reply, any specific sensor I can use for monitoring fuel level in Generator fuel tank, or start and stop on generator that can integrate with NetBotz. Regards, Felix.

(CID:105471443)

Reply

Link copied. Please paste this link to share this article on your social media post.

DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2024-04-09 12:28 AM

In response to DCIM_Support
0 Likes
0
1119
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
Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2024-04-09 12:28 AM

Hi Felix, We don't have any specific sensors for that. I have not worked with any myself either but perhaps someone watching this post has. Any 0-5v or 4-20ma sensors should work. Steve

(CID:105471444)

Reply

Link copied. Please paste this link to share this article on your social media post.

DCIM_Support
Picard DCIM_Support
Picard

Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2023-10-31 10:15 PM

0 Likes
0
1119
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
Posted: ‎2020-07-03 01:49 AM . Last Modified: ‎2023-10-31 10:15 PM

superhero.png

This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.