Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-03-21 03:39 AM
Hello,
I would be very happy if somebody has a configuration example for the following behaviour. I need to know if it is possible when a signal quality is changed from "good"(198) to "uncertain"(68...88) or from "good"(198) to "bad"(4...32) that then this signal raise as a alarm and this signal go into the alarm list. This I need to know for IEC60870 points.
Best regards
Alois
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-03-23 05:42 PM
If you're talking one or two points to monitor (per device), you could just write some logic that executes on input processed, tick the execute on quality change, and handdress a digital output to normal/alarm as necessary to generate an alarm on an internal digital point.
This isn't scalable however.
Doing this with every point would double your point count, or you could output to a single internal point per device to flag something has a bad quality. You could use some logic and SQL to dynamically handle the points on the device, but you would need to be careful on the performance impact (depending on your system you might have to run this fairly infrequently which may impact the usefulness of the alarm?)
I'm not aware of anything special in the IEC60870 protocol that might help here.
In your situation what is the cause of the points going bad that isn't already alarms such as OS connection failure? Maybe the system can detect the issue rather than the consequence and be quicker/better performance.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-03-23 05:42 PM
If you're talking one or two points to monitor (per device), you could just write some logic that executes on input processed, tick the execute on quality change, and handdress a digital output to normal/alarm as necessary to generate an alarm on an internal digital point.
This isn't scalable however.
Doing this with every point would double your point count, or you could output to a single internal point per device to flag something has a bad quality. You could use some logic and SQL to dynamically handle the points on the device, but you would need to be careful on the performance impact (depending on your system you might have to run this fairly infrequently which may impact the usefulness of the alarm?)
I'm not aware of anything special in the IEC60870 protocol that might help here.
In your situation what is the cause of the points going bad that isn't already alarms such as OS connection failure? Maybe the system can detect the issue rather than the consequence and be quicker/better performance.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.