Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

[Imported] Indirect addressing

EcoStruxure Geo SCADA Expert Forum

Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
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
  • Remote Operations
  • EcoStruxure Geo SCADA Expert Forum
  • [Imported] Indirect addressing
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
sbeadle
sbeadle Champion
335
AndrewScott
AndrewScott
125
BevanWeiss
BevanWeiss
104
View All

Recommended Forums

  • Remote Operations Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to EcoStruxure Geo SCADA Expert Forum
Start a Topic
sbeadle
sbeadle Champion
Champion

Posted: ‎2019-11-05 01:54 PM . Last Modified: ‎2023-05-03 12:33 AM

0 Likes
0
1216
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
Posted: ‎2019-11-05 01:54 PM . Last Modified: ‎2023-05-03 12:33 AM

[Imported] Indirect addressing

>>Message imported from previous forum - Category:Scripts and Tips<<
User: mchartrand, originally posted: 2018-10-25 18:47:33 Id:271
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.

_______

**_tresleiv:
Is there a way to use indirect addressing by eg. point to a parameter string (or similar) from mimic expression where the parameter string contains the path of the actual point and returns current value of this point?_**

_______

AWoodland:
Yes, use indirect variables. Check the help but make sure you understand the details in the help on the performance impact of indirect variables.

What are you trying to do? There may be better, simpler and more efficient ways to do whatever you're trying to achieve. For example passing parameters into the mimic.

_____________

**_tresleiv:
We are trying to access a common parameter outside the template. This parameter is used widely internal in the template and it generates a lot of work if the name or path for the mentioned parameter changes. It is therfore much more convenient for us to use indirect adressing as we only have one point to change instead of editing 10 mimic expressions in the template.
Do you have an example code for an indirect addressing in mimic expression where it returns the actual value of target.
You mentioned something about passing parameters into the mimic, can you please elaborate?
Once again, thanks!_**

_______

AWoodland:
The help in ViewX will explain how to use parameters, and provide a number of examples, as it is basic mimic functionality. If you attend a mimic training course they'll also go through how to use them.

Even if you 'hardcode' the reference to the object outside the mimic it should still update if you move or rename it. It sounds like you're basically trying to create an object (I assume in a static location) to reference a potentially dynamic location for the template to then reference. If so you're making this much more complex than you need and the database should handle any changes to the referenced object for you (different if you delete and add as the link is lost).

You might also look at using formulas in property overrides in your templates, that may also achieve what you may be trying to do.

______________

richie133:

The easiest way to achieve this by using logic (ST, FBD, etc.)


Sometimes I use function block (Create New Logic Function Block Diagram) to do this.

So first assume you have physical / generic analog point, then you can create internal analog point (Create New Internal Analog Point).

You only need to drag this two points and put that on the Direct tag of FBD, then you drag the generic analog point as input variabel, internal analog point as output variable, and last just connect them with line. That will do the trick.

 

If you want the point to be fast updated, just change the execution interval like less than 0.5S (500 miliseconds)

Labels
  • Labels:
  • SCADA
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.