Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Search in
Please select a country to continue with beta search.
Posted: 2021-12-20 08:37 PM . Last Modified: 2023-05-02 11:59 PM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-12-20 08:37 PM . Last Modified: 2023-05-02 11:59 PM
Good day,
i know it's a very simple question and it makes with about dozen clicks, but i'm just started you learn GeoSCADA and i've got a problem
Can anyone describe me what should i do to send data of one point to another with IEC-104 using only one PC (GeoSCADA Expert 2019)
Sincerely regards.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-12-21 01:33 PM
Do you have two outstations here, or are you just talking about a single outstation and the Geo SCADA Expert SCADA platform?
If you're trying to get two outstations to talk to each other, then you should NOT involve Geo SCADA Expert.
Have one be the master, and the other the slave in such a connection.
The master for the peer-to-peer communications in the situation above could still be a slave for the communications to Geo SCADA Expert.
If you're just communicating from Geo SCADA Expert to a single outstation, then you'd want to be using the IEC60870-5 objects (Channel, Outstation Set, Outstation) and then either an Analog Output or a Digital Output point configured to suit the IOA of the point on the outstation in question. This will then provide the Control method to allow for changing the values.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-12-21 01:33 PM
Do you have two outstations here, or are you just talking about a single outstation and the Geo SCADA Expert SCADA platform?
If you're trying to get two outstations to talk to each other, then you should NOT involve Geo SCADA Expert.
Have one be the master, and the other the slave in such a connection.
The master for the peer-to-peer communications in the situation above could still be a slave for the communications to Geo SCADA Expert.
If you're just communicating from Geo SCADA Expert to a single outstation, then you'd want to be using the IEC60870-5 objects (Channel, Outstation Set, Outstation) and then either an Analog Output or a Digital Output point configured to suit the IOA of the point on the outstation in question. This will then provide the Control method to allow for changing the values.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-12-21 10:34 PM
Thank you very much! I did it.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.