Schneider Electric support forum about installation, configuration, integration and troubleshooting of EcoStruxure Geo SCADA Expert (ClearSCADA, ViewX, WebX).
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-01-1703:52 PM. Last Modified: 2023-05-0211:59 PM
How ViewX Server Licenses are supposed to work?
Hello,
I'm wondering how many ViewX clients we can connect to Main-Standby system when both servers have an equal amount of ViewX licenses, e.g. 10 ViewX licenses each as it appears in the License Details window on both servers. Should that allow 10 or 20 ViewX clients to connect to the system? and what if the Main server has a different amount of licenses than the Standby one? e.g. Main server has 8 and standby has 10 ViewX licenses.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-01-1708:44 PM
If you have paid for full floating client licences, then you would have purchased 20x such licences, and hence would be allowed to operate 20 clients from this arrangement.
If you're not seeing this, then you should contact your local Tech Support branch to investigate further.
The clients would need to be configured to allow server floating licences of course.
If you have only purchased 10x full licences and the other 10x are redundant client licences, then you should only allow 10 clients to use these licences at any one time. However I don't believe there is a technical limitation here, I'm pretty sure the redundant client licence still appears as a standard client licence within the dongle / soft key licence information.
It is just a legal limitation, so if you were ever audited as to your licence usage, and it revealed you had more active clients than full purchased client licences then you would be in breach of the EULA and would likely have your licences revoked, and would be pursued for civil damages (sued for breach of contract / breach of copyright... whatever the vendor could get to stick).
Lead Control Systems Engineer for Alliance Automation (VIC). All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..