Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84796members
354245posts

Add menu option to map context sensitive menu. GeoScada

EcoStruxure Geo SCADA Expert Forum

Find out how SCADA systems and networks, like EcoStruxure Geo SCADA Expert, help industrial organizations maintaining efficiency, processing data for smarter decision making with IoT, RTU and PLC devices.

brcgomezle
Crewman
Crewman

Add menu option to map context sensitive menu. GeoScada

Hi,

 

Is there a way to add a menu option to the map context sensitive menu in the same way that can be added to the alarm banner context-sensitive menu? 

 

The scripting guide explains the process to add a menu using the function "AlarmBanner.AddMenuItem".

 

What is the function to add the custom menu?

 

Thanks for your help

 

 

 

1 Reply 1
BevanWeiss
Spock
Spock
0 Likes
0
881

Re: Add menu option to map context sensitive menu. GeoScada

I don't believe there is an easy way to add a Menu Option on the map.  Although I haven't tried this exactly.

 

The Alarm Banner is the most flexible with the scripting capability.  It is also possible to add Context Menu options in general locations, but these are more restricted to just additional data queries

 

 

It seems my screenshot copy-paste isn't working in this forum today.  But I've attached a screenshot showing where such an additional data query could be added.. and the kind of thing that it would be for.

 

I'd recommend having a look through the current 'Feature Request' list to see if the item you want is already there.. and if so add your vote and potentially add your comment to ensure that your particular use case is documented alongside the existing request.

 

https://community.exchange.se.com/t5/Geo-SCADA-Expert-Ideas/idb-p/geo-scada-expert-ideas

 


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
Attachments