Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Send New InviteClose
Announcements
Find the latest Product Announcesments on The Exchange here: PA-00941 - EcoStruxure Building Advisor - New Features Q2 2023
Enhanced Mode is for b3 controllers only. Therefore, there should be a recommendation to change the setting for the following conditions:
If MSTP Comm Port has all b3 controllers, then Enhanced Mode should be TRUE.
If there are no b3 controllers on that MSTP Comm Port, then Enhanced Mode should be FALSE.
If there is a mix of b3 and other BACnet devices, then either position could improve or worsen communications, so it does not need to be included in a recommendation.