Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Send New InviteClose
Announcements
Find the latest Product Announcesments on The Exchange here: PA-00941 - EcoStruxure Building Advisor - New Features Q2 2023
BACnet IP port should be checked and reported if IP Port - Broadcast Address is 255.255.255.255, which indicates a misconfiguration. Since the IP ports are setup by IP Address and not Adapter, one has to change the IP Address of the Port, when the IP Address of the adapter changes. If this is not done, the calculated Broadcast Address will show 255.255.255.255 instead of the correct value based on adapter IP address and Subnet Mask.