Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84525members
353768posts

M262 & MQTT & CAN?

EcoStruxure Automation Expert / IEC 61499 Forum

Browse this forum to find everything you want to know about EAE and IEC 61499 for distributed control systems. Ask experts your questions, get answers, discuss, and share your experience with the growing community.

Solved
DP-JYC
Lieutenant JG
Lieutenant JG
0 Likes
3
682

M262 & MQTT & CAN?

I'm a big fan of IEC61499 and I presented it to multiple End Users.
They are really enthousiaste about it, but they had a few questions that could be linked to your roadmap.

 

Let me put it here; 

  • When will M262 be able to be managed by EcoStruxure Automation Expert running IEC61499?
  • Do you have an MQTT library available? If not when?
  • Do you have a CAN library available? If not when?


Thank you for your answers

Tags (1)

Accepted Solutions
DP-JYC
Lieutenant JG
Lieutenant JG
0 Likes
1
674

Re: M262 & MQTT & CAN?

Thanks so much for your quick and informative reply.

 

The End User dosen't know much about automation and was convinced about EcoStruxure Automation Expert after my presentation 😎.

 

As it's very project project specific we should probably connect directly?

I will send you a mail.

See Answer In Context

Tags (1)
3 Replies 3
Kaishi
Ensign Ensign
Ensign

Re: M262 & MQTT & CAN?

Hello DP-JYC:

 

Thanks for being an ambassador of EcoStruxure Automation Expert and a valuable member of this community.

 

To answer your questions:

- The plan of Modicon M262 controller is being investigated as we speak. It would be very helpful for us to understand the exact customer need, or the reasons why the need could not be fulfilled by current dPAC platforms.

 

- MQTT support is currently being planned for V22.0 in April 2022.

 

- For CAN Open, we would love to get in touch with you to groom and provide a solution if you have specific project needs.

 

     

Tags (1)
DP-JYC
Lieutenant JG
Lieutenant JG
0 Likes
1
675

Re: M262 & MQTT & CAN?

Thanks so much for your quick and informative reply.

 

The End User dosen't know much about automation and was convinced about EcoStruxure Automation Expert after my presentation 😎.

 

As it's very project project specific we should probably connect directly?

I will send you a mail.

Tags (1)
Kaishi
Ensign Ensign
Ensign
0 Likes
0
670

Re: M262 & MQTT & CAN?

You are welcome and look forward to connecting with you.

Tags (1)