Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Device view features
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • Data Center Expert
  • DCE Device and Map views
  • Device view features
Options
  • My Knowledge Base Contributions
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support

Device view features

Sort by:
Views
  • Date
  • Views
  • Likes
  • Comments
  • Helpfulness
Options
  • Subscribe
  • Bookmark
  • Invite a Friend

Information columns

The Device View columns provide information and status for listed devices.   A Configure Columns icon at the top of the view allows you to define which columns are displayed.   Column Description Type The type of device, with SNMP Device used as a generic identification. Status The severity of the most serious alarm condition at a device. Note: You can select a device in the Device View to access information about its alarms in the Active Alarms view. Monitored SNMP devices typically report three status conditions: Normal: no alarm conditions exist. Warning, a condition exists that may require attention to make sure it does not deteriorate into a critical state. For example, a UPS that is running on battery power during a power failure will shut down its load equipment if its battery power is depleted before power returns to normal. Critical: a condition exists that requires immediate attention. For example, a discharged battery can result in the loss of UPS protection during a power failure. NetBotz Appliances typically report two status conditions, in addition to Normal: Error: a sensor threshold violation exists that requires immediate attention. For example, a high temperature violation that could lead to equipment damage. Failure: an operational failure exists that requires immediate attention. For example, communication with a camera pod was lost which could lead to an undetected security violation. Note: The status reported for alert threshold violations can be defined by the severity settings for each threshold. For example, a door sensor can be set to report Informational status for an open door. Model The device model, if known. For example, Silcon DP310E, for an APC UPS. Hostname The hostname, or IP address, if no hostname is defined, for a monitored SNMP device or NetBotz Appliance. Note: A Hostname is provided for SNMP devices monitored by NetBotz Appliances, but not for non-SNMP devices such as sensor and camera pods. Parent Device Identifies the Data Center Expert server, for SNMP devices directly monitored by the server, or the hostname or IP address for a NetBotz Appliance and its supported devices. Serial Number The serial number assigned to a device, if known. IP Address The IP address used by a monitored SNMP device or NetBotz Appliance. Note: An IP Address is provided for SNMP devices monitored by NetBotz Appliances, but not for non-SNMP devices such as sensor and camera pods. Location The location associated with a device, if known. Application Version The application or firmware version number for a device, if known. Label The label defined for a device. Maintenence Mode Indicates a device is in Maintenance Mode, and alarm notifications for that device have been disabled (Yes), or not in Maintenance Mode, and alarm notifications are enabled (No), the default. Groups The names of any device groups a device belongs to, including All Devices and Unassigned. MAC Address The unique network interface identifier for the device. Contact Name The name of the contact associated with the device.    
View full article
Picard EcoStruxureIT
‎2019-11-20 06:14 AM

Last Updated: Sisko JLehr Sisko ‎2024-02-14 10:04 AM

2015 Views

NetBotz Appliances in the Device View

A NetBotz Appliance appears in the Device View as an expandable listing. When expanded, each device it monitors is listed under the main NetBotz Appliance listing, including an entry that reports the network status of the appliance itself.   The hostname or IP address of the NetBotz Appliance is reported in the Parent Device column for the NetBotz Appliance, and for each associated device. You can select the right-click View Device Sensors for the main (expandable) listing for a NetBotz Appliance in the Device View (or for a NetBotz Appliance icon in the Map View), to access information about all sensors for the NetBotz Appliance and any devices that it monitors. You can double-click the main NetBotz Appliance entry, or from any of its associated devices, to launch to the appliance's web interface (or highlight the appliance in the Device View or Map View and select the right-click Launch to Device option). You can right-click a main NetBotz Appliance entry to connect to that device using Advanced View (right-click Launch Advanced View option) Note: This option must be enabled in File > Client Preferences > Advanced View Settings. If the NetBotz Appliance is on the Data Center Expert server's private network, SOCKS Proxy must be enabled in System > Server Administration Settings>Server Access > Socks Proxy, and you must be a Data Center Expert Administrator, or a user with the Data Center Expert Proxy role assigned. You can right-click a main NetBotz Appliance entry, or any of its Rack Access 170 devices, to lock or unlock rack doors using the Rack Access Control option. Note: The Rack Access Control option is available only when a Rack Access Pod 170 is connected to the selected NetBotz Appliance. You can move copies of any associated device, including the device that represents the appliance, to any other device group; a copy of that device remains associated with the main NetBotz Appliance listing.
View full article
Picard EcoStruxureIT
‎2019-11-20 06:14 AM

Last Updated: Sisko JLehr Sisko ‎2024-01-31 01:13 PM

1492 Views

Device View features

This view uses a table format to provide access to information about the monitored devices. It also is used to manage which devices are assigned to which device groups, a function that cannot be performed in a Map View.   The File > Client Preferences > Device View Settings > Total Devices Shown setting defines the maximum number of devices that can be listed in the Device View at any one time (500, by default). You can select the Highlight Priority Alarms setting to have devices with active Critical, Error, and Failure alarms highlighted in red in the Device View (disabled, by default).   In addition to managing the devices in the device groups, the Device View has the following features:   The device list provides information about each device in the device group selected in the Device Groups view. You can click the Configure Columns icon to define which columns appear in the view. You can click a column title to sort the list in ascending or descending order based on the information in that column. A Search field and Clear button allow you to filter the device list to display only the devices that include your typed text. You can select a device, or devices, to filter the Active Alarms view to show only the alarms for selected devices. Note: When a NetBotz Appliance is selected, the Active Alarms view will display its alarms, including all alarms associated with the devices it monitors. You can double-click a device to log on to its web interface, if it has one, or use the right-click Launch to Device option for a device. Note: By default, the web interface of devices requiring basic authentication is displayed as a view using the internal web browser. You can use the Launch in External Browser icon in that view to log on to the web interface in an external browser. Right-click options, and icon buttons at the top of the view, perform the following functions: Initiate a device discovery process used to add SNMP devices, Modbus devices, or NetBotz Appliances to be monitored by the Data Center Expert server (Add Devices option or the green + icon). Delete devices that you no longer want the Data Center Expert server to monitor (Delete Devices option or the x icon). Note: This option is disabled for a device that has a NetBotz Appliance as its parent device. Generate a report or graph for the historical values of the sensors at selected devices (Generate Sensor History Report option or Generate Custom Sensor History Report icon). Access the Alarm History view to review historical alarm data for any selected devices (Show Alarm History option). Define the port and protocol settings, and the username and password to be used by the Data Center Expert server to communicate with monitored devices (Device Launch Settings option). Note: For monitored APC SNMP and Modbus devices, the default username and password "apc" is provided by default. Control the outlets at a selected APC Rack PDU device (Outlet Control option). Log on to the web interface at a selected device, if it has one (Launch to Device option). Log on to the Advanced View interface at a selected NetBotz Appliance (Launch Advanced View option). Note: This option is enabled by Advanced View Settings, a Client Preferences option in the File menu. Remove selected devices from a shared device group, without causing the Data Center Expert server to stop monitoring those devices (Remove Device from Group option). Request that the Data Center Expert server immediately scan selected devices for sensor values, without waiting until the server would normally scan those devices (Request Device Scan option). Note: This option is enabled by Advanced View Settings, a Client Preferences option in the File menu. View all the values being reported by the sensors at selected devices (View Device Sensors option). Select the appropriate device type for a third party device, or more accurately define an SNMP device (Change Device Type option). Configure the device to use its defualt label or specify a custom label (Device Label Settings option). Create thresholds for a selected device, or set of devices. See Threshold Alarm Configuration view for more information. Configure selected APC SNMP devices to use the same values for shared settings (APC SNMP Device Configuration option). Note: An APC SNMP Device Configuration option is also in the Device menu. For information about these options, see APC SNMP Device Configuration. Access an option to lock or unlock rack doors using the Rack Access Control option for a main NetBotz Appliance, or any of its associated Rack Access Pod 170 devices. Note: The Rack Access Control option is available only when a Rack Access Pod 170 is connected to the selected NetBotz Appliance. Access a specific configuration option for a selected NetBotz Appliance or camera pod (NetBotz Appliance Configuration options). Note: A NetBotz Appliance Configuration option is also in the Device menu. For information about these options, see NetBotz Appliance Configuration. Access the Surveillance perspective with a selected camera highlighted in the Thumbnails view (Show in Surveillance Perspective option). Show in Surveillance Perspective is only available when a camera is selected; when multiple cameras are selected, only the camera closest to the top of the Devices View is highlighted in the Thumbnails view. Disable or re-enable notifications for any SNMP or Modbus device, or device group (Enter/Exit Maintenance Mode options). Create a custom property, or edit the value of an existing property, for the selected devices or sensors (Add Custom Property option). Access the Custom Properties Editor view to add, modify, or remove custom properties for selected devices or sensors (Open Custom Properties Editor option). Create a virtual sensor for a selected device, or set of devices (Create Virtual Sensor option). See Virtual Sensors view for more information.  
View full article
Picard EcoStruxureIT
‎2019-11-20 06:14 AM

Last Updated: Sisko JLehr Sisko ‎2024-01-31 01:11 PM

788 Views
Didn't find what you are looking for? Ask our Experts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.