Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Information columns

Device view features
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • Data Center Expert
  • DCE Device and Map views
  • Device view features
  • Information columns
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
  • NetBotz Appliances in the Device View
  • Information columns
  • Device View features
  • NetBotz Appliances in the Device View
  • Information columns
  • Device View features

Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support
Back to Device view features
Start a Topic
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2017 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Information columns

Picard EcoStruxureIT
‎2019-11-20 06:14 AM

Last Updated: Sisko JLehr Sisko ‎2024-02-14 10:04 AM

The Device View columns provide information and status for listed devices.

 

A Configure Columns icon at the top of the view allows you to define which columns are displayed.

 

Column Description
Type The type of device, with SNMP Device used as a generic identification.
Status

The severity of the most serious alarm condition at a device.

Note: You can select a device in the Device View to access information about its alarms in the Active Alarms view.

Monitored SNMP devices typically report three status conditions:

Normal: no alarm conditions exist.

Warning, a condition exists that may require attention to make sure it does not deteriorate into a critical state. For example, a UPS that is running on battery power during a power failure will shut down its load equipment if its battery power is depleted before power returns to normal.

Critical: a condition exists that requires immediate attention. For example, a discharged battery can result in the loss of UPS protection during a power failure.

NetBotz Appliances typically report two status conditions, in addition to Normal:

Error: a sensor threshold violation exists that requires immediate attention. For example, a high temperature violation that could lead to equipment damage.

Failure: an operational failure exists that requires immediate attention. For example, communication with a camera pod was lost which could lead to an undetected security violation.

Note: The status reported for alert threshold violations can be defined by the severity settings for each threshold. For example, a door sensor can be set to report Informational status for an open door.

Model The device model, if known. For example, Silcon DP310E, for an APC UPS.
Hostname

The hostname, or IP address, if no hostname is defined, for a monitored SNMP device or NetBotz Appliance.

Note: A Hostname is provided for SNMP devices monitored by NetBotz Appliances, but not for non-SNMP devices such as sensor and camera pods.

Parent Device Identifies the Data Center Expert server, for SNMP devices directly monitored by the server, or the hostname or IP address for a NetBotz Appliance and its supported devices.
Serial Number The serial number assigned to a device, if known.
IP Address

The IP address used by a monitored SNMP device or NetBotz Appliance.

Note: An IP Address is provided for SNMP devices monitored by NetBotz Appliances, but not for non-SNMP devices such as sensor and camera pods.

Location The location associated with a device, if known.
Application Version The application or firmware version number for a device, if known.
Label The label defined for a device.
Maintenence Mode Indicates a device is in Maintenance Mode, and alarm notifications for that device have been disabled (Yes), or not in Maintenance Mode, and alarm notifications are enabled (No), the default.
Groups The names of any device groups a device belongs to, including All Devices and Unassigned.
MAC Address The unique network interface identifier for the device.
Contact Name The name of the contact associated with the device.

 

 
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.