Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Configure 1 minute polling in EcoStruxure IT Gateway

Configuration

Detailed instructions for how to configure the EcoStruxure IT Gateway
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • Gateway
  • Configuration
  • Configure 1 minute polling in EcoStruxure IT Gateway
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
  • File transfer status sensor on EcoStruxure IT Gate...
  • Video: Configure Gateway device file transfer sett...
  • Video: Configure device credentials in the Gateway
  • Configure Gateway device polling
  • Configure 1 minute polling in EcoStruxure IT Gatew...
  • Configure Gateway backup
  • Configure Gateway restore
  • Configure SNMP trap ports
  • Trap receiver registration for third party devices
  • Configure SNMPv3 traps and informs in the Gateway
  • Connect PowerChute Business Edition agents (PCBE) ...
  • EcoStruxure IT Gateway logs
  • Configure Web credentials in the Gateway
  • File transfer status sensor on EcoStruxure IT Gate...
  • Video: Configure Gateway device file transfer sett...
  • Video: Configure device credentials in the Gateway
  • Configure Gateway device polling
  • Configure 1 minute polling in EcoStruxure IT Gatew...
  • Configure Gateway backup
  • Configure Gateway restore
  • Configure SNMP trap ports
  • Trap receiver registration for third party devices
  • Configure SNMPv3 traps and informs in the Gateway
  • Connect PowerChute Business Edition agents (PCBE) ...
  • EcoStruxure IT Gateway logs
  • Configure Web credentials in the Gateway

Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support
Back to Configuration
Start a Topic
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
6055 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Configure 1 minute polling in EcoStruxure IT Gateway

EcoStruxureIT
‎2021-10-01 01:16 AM

Starting with version 1.13 and newer, EcoStruxure IT Gateway can be configured to poll up to 25 devices at 1 minute instead of the normal 5 minute polling rate.

To select which devices will be polled at 1 minute:

  • Log into the Gateway and click Devices.

  • Click Edit polling interval… 

  • Under Choose polling interval, select 1 minute.

  • Select the devices you want to poll at 1 minute.

  • Click Apply.

To revert back to the 5 minute polling rate, follow the same instructions, and choose 5 minutes instead.

Gateway_1_440829733595313_one_minute_polling.gifGateway_1_440829733595313_one_minute_polling.gif

Limitations

  • Certain devices might not be able to poll at the 1 minute interval because the device requires more than 1 minute for a single complete poll. This is often the case when there are more than one device at an IP address, for example, an rPDU using Network Port Sharing (NPS).

    Note: For rPDUs using Network Port Sharing, the guest devices poll at the same rate as the host device. The Gateway application allows you to set the poll rate for guest devices, but it will have no effect.

  • Although the Gateway allows a maximum of 25 devices to poll at 1 minute, it may not be possible to poll that many on your system. The practical limit depends on the total number of devices being polled, the amount of CPU and memory on your Gateway, and the protocols used.

    SNMPv3 is significantly slower than SNMPv1 and Modbus TCP. For more information, see Gateway System Requirements. 

    • Medium and large Gateway configurations (more than 8 CPUs and 8 GB RAM) had no issues with the maximum configuration of 25 SNMPv3 devices polling at 1 minute. In a small Gateway configuration, 10 out of 60 SNMPv3 devices can be polled at 1 minute.

    • The small configuration (4 CPUs and 4 GB RAM, which also applies to the EcoStruxure IT Gateway NUC  appliance, INNUC0119) can poll 10 out of 60 SNMPv3 devices at 1 minute.

Alarms

Setting devices to poll at 1 minute may trigger a Device Communication Alert alarm if the Gateway cannot poll the device at that rate. 

 

Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.