Issue
What type of communications cabling is recommended for Arcnet and Sigma LANs?
Product Line
Satchwell SigmaEnvironment
Satchwell Sigma
Cause
Proper cable selection is essential to ensure reliable Sigma communication.
Resolution
For Sigma LAN communications, the following cable specifications are recommended:
-
Standard One-Pair Communications:
Use Belden 8762 or an equivalent cable. - Isolated LAN Communications:
Use Belden 9502 or an equivalent cable.
Supporting Documentation:
Additional Notes:
- Ensure cable installation follows manufacturer guidelines and local standards.
- Equivalent cables must match electrical and shielding characteristics of the recommended Belden models.
- Refer to the Satchwell Sigma Cabling Guide for further information