Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

What is the replacement for a Drayton Theta YBL1A Valve Body / Actuator assembly?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • What is the replacement for a Drayton Theta YBL1A Valve Body / Actuator assembly?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Product_Support
    Product_Support
  • CraigEl
    CraigEl

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
10946 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

What is the replacement for a Drayton Theta YBL1A Valve Body / Actuator assembly?

Picard Product_Support
‎2018-09-10 12:17 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-14 06:45 PM

Issue

The Drayton Theta YBL1A Valve Body / Actuator assembly is to be replaced.

Product Line

Field Devices

Environment

  • Replacement
  • Drayton
  • Actuator
  • Valve
  • YBL1A

Cause

The Drayton Theta YBL1A Valve Body / Actuator assembly is obsolete.

Resolution

OVERVIEW

The Drayton Theta YBL1A Valve Body / Actuator assembly is obsolete, and there is no purpose built replacement.

The Valve Body was available in 1.1/4", 1.1/2" and 2" B.S.P. sizes and was normally installed as a mixing valve in variable temperature, constant volume, compensated heating circuits.

No Valve Body / Actuator assemblies are currently available in these sizes.

Details of the YB Valve Body may be viewed here.

 

VALVE BODY REPLACEMENT

To replace the YBL1A Valve Body the following is required:-

S-E SatchwellMB Valve Body of appropriate size - MB1552 (1.1/4"), MB1602 (1.1/2"), MB1652 (2")

Details of the MB Valve Body may be viewed here.

 

ACTUATOR REPLACEMENT (6-WIRE INSTALLATION)

The YBL1A Actuator normally comprised a 6-wire electrical connection enabling it to be operated by a Theta Potentiometric Controller as follows :- 

Terminal M1 – Open signal

Terminal M2 – Close signal

Terminal M3 – Common 

Terminal M4 – 135 ohm Feedback Potentiometer – winding

Terminal M5 – 135 ohm Feedback Potentiometer – wiper

Terminal M6 – 135 ohm Feedback Potentiometer – winding

Where 6 wires are connected to the YBL1A Actuator then the Actuator may be replaced by one or other of the following S-E Actuators :-

MD10B-24

MD20B-24 (if MD10B-24 not available)

Details of the MD10B-24 Actuator may be viewed here

Details of the MD20B-24 Actuator may be viewed here.

N.B.

The YBL1A Actuator also included an additional 3-wire electrical connection associated with an integral S.P.C.O. Auxiliary Switch wired as follows :- 

Terminal S1 – Normally Closed Contact

Terminal S2 – Common

Terminal S3 – Normally Open Contact

Where external wiring is connected to the YBL1A Actuator Auxiliary Switch then an Auxiliary Switch Kit containing a S.P.C.O. Auxiliary Switch should be installed on the MD Actuator.

Auxiliary Switch Kit MD-S1 (914-1060-000)

Details of the MD-S1 Auxiliary Switch Kit may be viewed here.

The MD-S1 Auxiliary Switch Kit should be wired as follows :-.

Terminal S1 – Common

Terminal S2 – Normally Closed Contact

Terminal S3 – Normally Open Contact

 

LINKAGE KIT

A Linkage Kit will also be required in order to enable the MD Actuator to be mounted on the MB Valve Body.

Linkage Kit LMD/AR-MB (914-1071-000)

Details of the LMD/AR-MB Linkage Kit may be viewed here

 

IMPORTANT NOTE

In such 6-wire installations not only will the YBL1A Valve / Actuator assembly need to be replaced but the associated Theta Potentiometric Controller and its Sensors will also need to be replaced.

 

CONTROLLER REPLACEMENT

The Theta Potentiometric Controller may be replaced by the S-E Satchwell CSC5252 or the CSC5352 Compensator Controller.

Details of the CSC Controllers may be viewed here.

 

SENSOR REPLACEMENT

Theta 3-wire Temperature Sensors may be replaced by S-E Satchwell 2-wire Temperature Sensors compatible with the S-E Satchwell CSC 5252 or CSC5352 Compensator Controllers selected from the following as appropriate.

Outside Air Temperature Sensor (STO 600)

Contact Temperature Sensor (STC 600), or alternatively :-

Immersion Temperature Sensor (STP 660) + Sensor Pocket Adaptor (DWA 0001)

Room Temperature Sensor (STR 600) – OPTIONAL ONLY

Details of the STO 600 Outside Air Temperature Sensor may be viewed here.

Details of the STC 600 Contact Temperature Sensor may be viewed here.

Details of the STP 660 Water Temperature Sensor may be viewed here.

Details of the DWA 0001 Sensor Pocket Adaptor may be viewed here.

Details of the STR 600 Room Temperature Sensor may be viewed here.

 

N.B.

ACTUATOR REPLACEMENT (3-WIRE INSTALLATION)

Should only 3 wires be connected to a YBL1A Actuator then the Actuator may be replaced by one or other of the following S-E Actuators :-

MD10B-24

MD20B-24 (if MD10B-24 not available)

Details of the MD10B-24 Actuator may be viewed here.

Details of the MD20B-24 Actuator may be viewed here.

N.B.

The YBL1A Actuator also included an additional 3-wire electrical connection associated with an integral S.P.C.O. Auxiliary Switch wired as follows :- 

Terminal S1 – Normally Closed Contact

Terminal S2 – Common

Terminal S3 – Normally Open Contact

Where external wiring is connected to the YBL1A Actuator Auxiliary Switch then an Auxiliary Switch Kit containing a S.P.C.O. Auxiliary Switch should be installed on the MD Actuator.

Auxiliary Switch Kit MD-S1 (914-1060-000)

Details of the MD-S1 Auxiliary Switch Kit may be viewed here.

The MD-S1 Auxiliary Switch Kit should be wired as follows :-.

Terminal S1 – Common

Terminal S2 – Normally Closed Contact

Terminal S3 – Normally Open Contact

 

LINKAGE KIT

A Linkage Kit will also be required in order to enable the MD Actuator to be mounted on the MB Valve Body.

Linkage Kit LMD/AR-MB (914-1071-000)

Details of the LMD/AR-MB Linkage Kit may be viewed here

In such 3-wire installations the YBL1A Valve / Actuator assembly only will need to be replaced, while any associated Controller and Sensors may be retained.

Labels (1)
Labels:
  • Field Devices
Attachments
Tags (1)
  • Find more articles tagged with:
  • 5448
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.