Issue
Users may need to access the MicroNet LCD interface but are unsure of the default password required for initial login.
Product Line
Satchwell MicroNetEnvironment
- Satchwell MicroNet Controllers
- MicroNet LCD Interface
Cause
The default password is required to access the LCD interface. If it has been changed during programming, users may need to retrieve or reset it.
Resolution
-
Default Password:
1234
This is the factory-set password for MicroNet LCD interfaces. -
Password Change Considerations:
- The default password can be changed during controller programming.
- For 100 Series MicroNet controllers, if the password has been changed, a backup of the controller configuration is required to identify the current password.
- For 50 Series MicroNet controllers, when uploading the controller configuration, ensure the LCD configuration is also uploaded. The password can be found under Properties in the LCD configuration area.