Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

What are termination resistors and why use them?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • What are termination resistors and why use them?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • CraigEl
    CraigEl
  • sesa139513
    sesa139513
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
11838 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

What are termination resistors and why use them?

Product_Support
‎2018-09-06 03:23 PM

Last Updated: CraigEl Champion ‎2022-08-17 08:25 PM

Issue

What are termination (end of line) resistors and why use them?

A LAN of any type has a node or two somewhere in the middle having problems but the rest seem stable

Product Line

TAC INET

Environment

  • I/NET Site
  • Controller LAN
  • 7808 Repeater

Cause

Termination resistors (also called clamping or end-of line resistors) are to be installed between lan+ and lan -, not to ground. Their purpose is to prevent the characteristic impedance of the wire from increasing to infinity at the end of the cable.

Resolution

Since most wire's characteristic impedance is between 80 and 150 ohms, use 100 to 120 ohms on an unbiased controller or host lan. This will "clamp" reflections from the end of the wire which are seen as noise by the controllers.

If a 7808 repeater is used, it requires bias. Using 100 ohm termination resistors would kill that lan's communication; therefore, use 620 ohms instead.

As cheap as resistors are and as easy as this installation is, they can only help. Typically they help more on a longer LAN, so anything longer than 1000 feet (about 300 meters) should definitely have terminations.

Labels (1)
Labels:
  • TAC INET
Tags (3)
  • Find more articles tagged with:
  • 1252
  • eol
  • RobertAndriolo22
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.